KUKA Industrial Robots
KUKA Industrial Robots - Solutions database KUKA Industrial Robots - Solutions database
Downloads 
Contact 
KUKA Robot GroupSolutions
Company
Press/Events
Products
Solutions
Customer Services
Training
Sales

Custom-tailored solutions for your application

   

  Industry   Please select criteria for refining the results.  
  Application  
  Product  
  (*** = 100% match, ** = 66%, * = 33%)   Reset  

Robot plugs away
KUKA stainless steel robot screws stoppers into “Pittermännchen” barrels at Kölner Verbund Brauereien ...more
***
It is all a question of reliability
A KUKA robot drills and installs fasteners in aircraft components at Stork Fokker ...more
***
KUKA robots can handle everything
At Ciba Specialty Chemicals, KUKA robots palletize sacks of plastic additives. The desire to react even more flexibly to customer requirements prompted Ciba Specialty Chemicals, Basel (Switzerland), to invest in a state-of-the-art automation system. Two KR 180 PA-type KUKA robots ensure that the sacks of chemicals are stacked cleanly on pallets or in cartons. ...more
***
Can a car seat withstand conditions at the North Pole?
Car seats have to withstand a lot. The weight of the driver, for example, his movement while waiting impatiently at a red light, or extracting a wallet from his back trouser pocket.... ...more
***
Top quality in 13 minutes
At BOA AG, a KUKA robot welds not only quickly, but also with high quality. ...more
***
Robots bend large heavy metal plates
After hitting upon the idea of industrializing the building trade with the aid of prefabricated steel box panels, BSC began to search for an integrated automation solution for their production. The task was to prefabricate precision-fit elements in a large variety of shapes, sizes and widths. ...more
***
KUKA robots with integrated intelligence mean progress for the bending process
KUKA robots work alongside RAS MULTIBEND-CENTER in state-of-the-art production line. ...more
***
Robots take a shine to pot lids
KUKA robots grind and polish lids for pressure cookers and cooking pots for WMF.In an ultramodern, future-oriented system from SHL Automatisierungstechnik AG, WMF AG has turned to KUKA robot technology for grinding and polishing processes. ...more
***
Robots ensure good formwork
Three KUKA robots at Werzalit AG + Co KG perform important tasks in the manufacture of formwork elements.In addition to windowsills, which constitute the core business, Werzalit AG + Co KG also produces plywood, veneers, shaped industrial parts, bungs for the paper industry and formwork elements for the residential and industrial building sector. ...more
***
Handling of front and rear axles and car doors
For its Regensburg plant, BMW was looking to implement automation solutions for the handling of complete front and rear axles for the 1 Series and 3 Series, as well as for the handling of doors for these series. ...more
***

1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | 10 |

Latest Solutions

Robot plugs away

It is all a question of reliability

KUKA robots can handle everything

Can a car seat withstand conditions at the North Pole?

Top quality in 13 minutes