KUKA Industrial Robots
KUKA Industrial Robots - Solutions database KUKA Industrial Robots - Solutions database
Downloads 
Contact 
GermanySolutions
Company
Press/Events
Products
Solutions
Customer Services
Training
Sales

Custom-tailored solutions for your application

   

  Industry   Please select criteria for refining the results.  
  Application  
  Product  
  (*** = 100% match, ** = 66%, * = 33%)   Reset  

Grinding and polishing of implants
Aesculap’s benchmark factory in Tuttlingen manufactures high-quality implants. In the past, work in this field was primarily carried out manually. Then Aesculap wanted to optimize the entire process. The motivation to do this was strong pressure to reduce costs and the resultant desire for higher cost-effectiveness. ...more
***
Automatic bending of sheet metal
Previously, Metallkonzept Glaser GmbH used manual handling when bending sheet metal. In order to offer the bent parts at lower prices, the company was looking for a more cost-effective alternative. ...more
***
Bending of tubes
Since it is not possible to manufacture tube/hose/tube combinations in a single program cycle on conventional tube bending machines, Rosenberger AG was looking for a more flexible bending system which would at the same time provide outstanding precision, process reliability, and ease of operation. ...more
***
Handling of automotive safety parts
The die-casting company Eisenmann Druckguss wanted to automate the manufacture of flanges for electrical steering systems of cars – safety-related components, in other words. The special challenge in this case was that there was practically no tolerance with regard to repeatability. ...more
***
Dexterity to rival the human hand
For the series production of washing machine drums, the company Fried was looking for a solution that could guarantee a very high level of automation and high availability. All production cells used in the past for this kind of component were implemented with many manual activities and did not meet with the expectations of the company. ...more
***
Grips firmly in grip
Soft grips come today as standard on high-tech bottle crates. Production requires high quality automation as the basis for subsequent installation in the bottle crates. The HEKUMA automation system removes 8 soft grips per cycle and precisely positions and orientates them in transport pallets for further processing. ...more
***
Robot sorts and stacks packaged door frames
Ligmatech, a German specialist for automation systems in the wood processing industry, received an order for an automatic palletizing and sorting system for door frames. ...more
***
Handling of molds with KR 500
The company was looking for an automated solution for coating and handling the cores. ...more
***
Handling of dishwater housings
BSH Bosch und Siemens Hausgeräte relies increasingly on automation for the manufacture of its dishwashers. Therefore the company also planned to automate the application of bitumen sound-deadening pads to dishwasher housings. ...more
***
Handling of tiles
Previously this area involved manual operations. At that time each operator had to lift roof tiles weighing a total of 1.5 tonnes per day. This task was now to be automated. ...more
***

1 | 2 | 3 | 4 | 5 | 6 | 7 | 8 | 9 | 10 |

Latest Solutions

Robot plugs away

It is all a question of reliability

KUKA robots can handle everything

Can a car seat withstand conditions at the North Pole?

Top quality in 13 minutes

Solutions KUKA Germany

Grinding and polishing of implants

Automatic bending of sheet metal

Bending of tubes

Handling of automotive safety parts

Dexterity to rival the human hand