KUKA recieves major order from Spanish automotive parts supplier

KUKA Systems GmbH Augsburg won a major order from a Spanish car parts supplier in the second quarter of 2012, to build several highly flexible manufacturing lines

3. srpna 2012

The project comprises the entire engineering and construction for four lines that will manufacture car body parts such as front and rear sliding doors and tailgates for various types of vehicles. The contract includes building the pre-production assemblies. The order is valued in the lower double-digit million euro range.

Dr. Till Reuter, CEO of KUKA AG, says: "What's noteworthy about this product is the wide variety of models being assembled and the remote laser welding technology. The latter process enables parts to be welded from a considerable distance using a laser with a very high power density."

Nastavení cookie OK a objevovat KUKA

Tato webová stránka používá soubory cookie (více informací), aby Vám byl k dispozici optimální servis také on-line. Pokud naši webovou stránku dále používáte, aktivují se pouze technicky nezbytné cookies. Pokud kliknete na „OK a objevovat KUKA“, vyjadřujete svůj souhlas s použitím marketingových cookies. Kliknutím na „Nastavení cookie“ můžete zvolit, jaké cookies budou aktivovány.

Nastavení cookie