Volkswagen increasingly commits to KUKA technology

Volkswagen AG is increasingly committing to cutting edge technology from Augsburg. The company awarded a new frame contract for industrial robots to KUKA in the third quarter of 2012.

7. listopadu 2012

Important large order for KUKA Roboter

Under the terms of the contract, KUKA Roboter GmbH will supply in total 6,000 of its new KR QUANTEC generation of industrial robots, including KR C4 controllers, to various Volkswagen factories in Germany and Eastern Europe in 2013 and 2014. Of the total, 1,800 robots are destined for Emden and Zwickau, where they will be used on production lines for the VW Passat's successor. Audi AG will receive 2,600 units for the new Audi A4, which will be built at Ingolstadt und Neckarsulm. The remaining 1,600 units will be shipped to the Volkswagen plant in Bratislava, Slovakia. The orders from this blanket contract will be booked from now until 2014 as they are released by the customer. 

"We are proud that Europe's largest carmaker is increasingly committing to cutting-edge technology from Augsburg," said Dr. Till Reuter, CEO of KUKA AG, as he commented on the order placement. "After all, 6,000 robots is the highest number of units KUKA has ever received at one time in a blanket order."
 
Nastavení cookie OK a objevovat KUKA

Tato webová stránka používá soubory cookie (více informací), aby Vám byl k dispozici optimální servis také on-line. Pokud naši webovou stránku dále používáte, aktivují se pouze technicky nezbytné cookies. Pokud kliknete na „OK a objevovat KUKA“, vyjadřujete svůj souhlas s použitím marketingových cookies. Kliknutím na „Nastavení cookie“ můžete zvolit, jaké cookies budou aktivovány.

Nastavení cookie