Reduced assembly times with KMR iiwa and LBR iiwa

Thales Alenia Space builds satellites and develops components for civilian and military space technology. Shorter assembly times and effective use of labor: these are the goals of the “Tomorrow's Factory” project by Thales Alenia Space, which is scheduled to begin in the second half of the year.

21. května 2015

In cooperation with KUKA, the University of ENSAM and the integrator AKEO+, the Cannes, France-based company is working on an automated workstation employing two KUKA lightweight robots of the LBR iiwa type and a mobile platform. The robots and the autonomous platform are working in a clean room environment.

In this project, two robots will assemble components from different storage containers as part of a kitting application into a kit in preparation for the next step. The KMR (KUKA Mobile Robotics) iiwa is bringing the kit to the workstation to be mounted on the satellite. The company also plans to use a KMP omniMove transport platform to easily transport the delicate satellites from one station to another within the production room.

During the internal exhibition at Thales Alenia Space and thanks to the help of the University of ENSAM, a comparable smaller KUKA mobile platform was shown with the KUKA collaborating robot LBR iiwa. The platform's autonomous navigation system allows the robot to reach each storage container easily.

Nastavení cookie OK a objevovat KUKA

Tato webová stránka používá soubory cookie (více informací), aby Vám byl k dispozici optimální servis také on-line. Pokud naši webovou stránku dále používáte, aktivují se pouze technicky nezbytné cookies. Pokud kliknete na „OK a objevovat KUKA“, vyjadřujete svůj souhlas s použitím marketingových cookies. Kliknutím na „Nastavení cookie“ můžete zvolit, jaké cookies budou aktivovány.

Nastavení cookie