KUKA wins major systems engineering contract from U.S. automotive manufacturer

The project comprises the design and installation of a highly flexible manufacturing system to produce body components for a range of vehicle variants.

22. března 2018

KUKA Systems has won a substantial systems engineering contract from a major U.S. automotive manufacturer. The project comprises the design and installation of a highly flexible manufacturing system to produce body components for a range of vehicle variants. The order volume lies in the high double-digit-million euro range and was booked in the fourth quarter of 2017. The start of production is scheduled for 2019.

At the North American plant, automated joining processes are to be integrated into the line for the front structure, underbody and body framing of the vehicle. The line is to include the KUKA KS Framer, which can produce up to six different models.

“We are proud that we have once again been able to convince our customer with our high-tech products. At the same time, this order underscores the out-standing partnership between our two companies,” explains Dr. Till Reuter, CEO of KUKA AG.

 

Stáhnout aktuality

Nastavení cookie OK a objevovat KUKA

Tato webová stránka používá soubory cookie (více informací), aby Vám byl k dispozici optimální servis také on-line. Pokud naši webovou stránku dále používáte, aktivují se pouze technicky nezbytné cookies. Pokud kliknete na „OK a objevovat KUKA“, vyjadřujete svůj souhlas s použitím marketingových cookies. Kliknutím na „Nastavení cookie“ můžete zvolit, jaké cookies budou aktivovány.

Nastavení cookie