KUKA´s largest robot at Multicut
The largest KUKA installation in Denmark, and the industry’s largest robot: the KUKA robot KR 1000 titan is located at Multicut A/S in Vildbjerg, where it supports an FMS system with four CNC machining centers at the largest, heaviest end. There's also another KUKA robot for milling and deburring operations.
May 10, 2017
KUKA robot works with four CNC machining centers
The robot loads in one place, and at the same time, the three other centers are running. Therefore, machine capacity can be completely exploit. “We have fully utilized the KUKA robot’s control system, so we know that the workpiece is located correctly before machining, and post-control, when we take the workpiece out again”, says Hans Jørgen Gam.
Second KUKA robot for milling and deburring operations
The final station, before workpieces leave the FMS system, also includes another smaller KUKA robot that mills and deburrs the edges of the holes so they are completely smooth and ready for use. The milling and deburring robot uses the KUKA.ForceTorqueControl for the operation to compensate for large variations in the workpieces.
Get more information about KUKA.ForceTorqueSensor system. The technology package makes the use of KUKA industrial robot systems in sensitive robot applications possible. There`s also another KUKA robot for milling and deburring operations.