Mit 10.12. hat die KUKA CEE GmbH ihren neuen Firmensitz in Steyregg.

We have moved!

As of December 10, KUKA CEE GmbH's new headquarters will be located in Steyregg.

7 December 2018

KUKA CEE GmbH changed its location on 10 December 2018. The new company building now offers its own Application Center and an extended KUKA College. 

The new location is in the  

Gewerbeallee 12
4221 Steyregg


With this new larger company site, our customers now have the possibility to test your applications in advance with our engineering team in our in-house Application Center
We also offer an extended KUKA College with 6 training cells to our customers which will be ready for use as early as January. 
 

 

KUKA Application Center 

In the new KUKA Application Center in Steyregg, our application engineers are working on the latest robot technologies. There are 4 robot cells available covering the entire payload range from 6 to 270 kg. This enables us to carry out feasibility studies on specific problems for our customers and to solve them by using KUKA technology packages. With the Application Center, we are now able to advise our partners and customers comprehensively and competently in all technical matters - and not only on paper, but in practice.
 
Die KUKA CEE GmbH ihren neuen Firmensitz in Steyregg.
The new company building of KUKA CEE GmbH in Steyregg.

KUKA College

In a first step the KUKA College was expanded to 6 robot cells. This means that several training courses can be offered in parallel. Hence we are able to extend the training program and include additional courses for maintenance personnel and expert training for integrators and system partners. The new college building will provide space for a total of 9 training cells in the future. The high level of practical training with two participants per robot can thus be maintained. In the future, the KUKA College will also play a role in the training sector for schools and universities of applied sciences. Practical laboratory exercises can thus be carried out efficiently in the newly designed college as part of the KUKA Student concept.
Cookie settings OK and discover KUKA

This website uses cookies (find out more) in order to offer you the best service online as well. If you simply continue to use our website, we will only use cookies required for technical purposes. If you click on “OK and discover KUKA”, you are also agreeing to the additional use of marketing cookies. You can select which cookies we use by clicking on “Cookie settings”.

Cookie settings