You are using an outdated browser version of the Internet Explorers. Please update your browser for ideal presentation of the website.
A KUKA robot becomes a part of Dutch cultural history
The art group ‘robotlab’ installed a KUKA robot in the city of Dordrecht. There, it is transcribing the Bible. The art project is part of the festivities for the 400th anniversary of the Synod of Dordrecht – a seminal event in the history of Dutch Protestantism.
18 June 2019
The art group has existed since 2000. Their work examines the relationship between humans and robots. Since the group’s inception, Matthias Gommel, Martina Haitz and Jan Zappe have organized more than 100 exhibitions. The current ‘bios [bible]’ project is exhibited in the Dutch city of Dordrecht. The centerpiece there is a KUKA robot from the KR CYBERTECH series.
The KUKA robot independently transcribes the Bible in Dutch. To carry this out, it has been equipped with a specially developed spring-tension pen holder. It has an integrated calligraphy fountain pen which enables particularly beautiful writing. The fountain pen is connected to an external ink system. This ensures a continuous supply of ink and uninterrupted writing.
Equipped with special fountain pen, the robot transcribes the Bible.
Bible texts saved as digital files
The Bible text is loaded onto the controller in the form of special, computer-generated files. The writing style used by the KUKA robot from the KR CYBERTECH series is a calligraphy font developed especially for this project that was also specially generated and integrated into the controller software. The KUKA robot fills several scrolls with writing – each with a length of 200 meters. The full work of writing takes nine months.
Continuing page after page, the robot fills several paper scrolls with a length of 200 meters with writing.
Robot gives a nod to monks from the Middle Ages
The Bible-transcribing robot carries out its work in the context of the 400th anniversary of the Synod of Dordrecht. Dordrecht was the site of an important assembly from 1618 to 1619 during the Reformation in the Netherlands. At that time, the decision was taken to translate the Bible from Greek into Dutch. The work of transcription, at that time, was still often carried out by monks. Now, 400 years later, a robot is carry out this monotonous and highly detailed work.
Bios juxtaposes two underlying systems: Christianity and scientific rationalism. Here, writing has always played a special role, both for holy scripture and for the documentation of knowledge.
This website uses cookies (find out more) in order to offer you the best service online as well. If you simply continue to use our website, we will only use cookies required for technical purposes. If you click on “OK and discover KUKA”, you are also agreeing to the additional use of marketing cookies. You can select which cookies we use by clicking on “Cookie settings”.