With more than 1,700 KUKA robots: Volkswagen starts series production of the ID.4

On the heels of the ID.3, Volkswagen is starting production of its second fully electric vehicle: the ID.4. In 2021 alone, up to 300,000 electric vehicles for Volkswagen, Audi and Seat are to be produced in Zwickau based on Modular Electric Propulsion (MEB). More than 1,700 KUKA robots are involved in body-in-white production and assembly.

15 October 2020

For more than two years, KUKA has been working with the Volkswagen automotive group in Zwickau on the fully electric vehicles ID.3, ID.4 and further models. It was recently announced that the ID.4 will now go into series production. For the more than 1,700 KUKA robots in Zwickau, some of which are on linear traversing axes of the type KL 4000, this means a lot of work. 

KUKA robots also provide support in Volkswagen battery production

The KUKA robots are used in body-in-white production as well as assembly in Zwickau. For the most part, KR QUANTEC and KR FORTEC robots are at work in the plant, however, LBR iiwa robots are also involved. KUKA robots have also contributed to the scalable battery system of the Modular Electric Propulsion (MEB) vehicles – which can achieve a range of over 500 kilometers and are manufactured at the site in Braunschweig. “We are delighted to be part of Germany’s first purely electric automobile factory. Together with Volkswagen, we are working to drive electromobility and the future of the automotive industry forward,” says Peter Mohnen, CEO of KUKA AG.
Body-in-white production at the Zwickau plant: here, the side section of the Volkswagen ID.3 is being built with help from KUKA robots.

Purely electric production in Zwickau since July 2020

Up to the middle of this year, the Volkswagen model Golf Variant with an internal combustion engine was also manufactured in Zwickau. Those days are over. From now on, only electric vehicles will roll off the conveyor. Thanks to an investment of 1.2 billion euro, the plant will be completely converted to electromobility by the end of the year. In 2021, the first year of fully electric production, around 300,000 electric cars based on Modular Electric Propulsion (MEB) are to be produced in Zwickau. From 2022 onwards, up to 330,000 units per year are to be achieved. But production in Zwickau is not just to be limited to the ID.3, that is already available to customers, and the new ID.4: the plant is set up for a total of six different electric models from Volkswagen, Audi and Seat.

 


We are delighted to be part of Germany’s first purely electric automobile factory. Together with Volkswagen, we are working to drive electromobility and the future of the automotive industry forward

Peter Mohnen, CEO of KUKA AG
Cookie settings OK and discover KUKA

This website uses cookies (find out more) in order to offer you the best service online as well. If you simply continue to use our website, we will only use cookies required for technical purposes. If you click on “OK and discover KUKA”, you are also agreeing to the additional use of marketing cookies. You can select which cookies we use by clicking on “Cookie settings”.

Cookie settings