RoboGym: revolutionary training – not just for top athletes

What does the future of training look like? Can a robot be used for strength training to potentially achieve greater progress? To what extent is there acceptance of technology among the general population and among athletes?

16 November 2020

KUKA is doing pioneering work

KUKA has been working on these questions related to the topic of sports and robotics for a long time. At the end of 2014, the long-standing system partner, BEC, was added. BEC then presented the first “RoboGym” prototype at the start of 2015. The “RoSylerNT” research project began in 2017 in cooperation with RWTH Aachen and the German Sport University Cologne along with support from the German Federal Ministry of Education and Research. The so-called “RoboGym” is to be ready for the market quite soon and, in many respects, represents an improvement compared to conventional training methods. What was originally planned exclusively for use by top athletes could indelibly alter the way that we train in the future. 
This is what the future of training could look like.

The advantages of the RoboGym

While conventional strength training devices only allow for linear loads with a constant weight, the RoboGym based on the KR 160 nano makes entirely new motion geometries as well as focusing on individual muscle groups possible – all thanks to the biomechanical skeletal models stored in the database. Test persons have reported improved performance capacity and that they feel completely safe. The installed sensor system for force measurement as well as built-in safety features (such as safety spaces and velocity monitoring) make it possible – particularly in the field of rehabilitation, for example, after a torn cruciate ligament – to control the maximum load as well as the extent of movement for the individual areas in such a way that subsequent injuries are avoided and athletes return to their usual level more quickly.

RoboGym – The future of training

Safe and versatile

So far, the RoboGym supports three types of training. In addition to the leg press, there is a knee extension option as well as a rowing exercise for the upper body. The data are displayed on the screen in real time and saved in a Cloud. Upon activating the device, the data are called directly from anywhere in the world and the device adjusts to the height and desired training weight. The acquisition of the data enables significantly more precise screening in which the force actually applied as well as the movements during each part of the exercise can be seen even more precisely. This allows training to be adapted to individual requirements.

Leg press with sensors for force measurement and a screen with training data

Our dream is for the RoboGym to become the standard in professional sports and rehabilitation, and to be found in every Olympic training facility.

Martin Gerlich, CFO of BEC GmbH
Cookie settings OK and discover KUKA

This website uses cookies (find out more) in order to offer you the best service online as well. If you simply continue to use our website, we will only use cookies required for technical purposes. If you click on “OK and discover KUKA”, you are also agreeing to the additional use of marketing cookies. You can select which cookies we use by clicking on “Cookie settings”.

Cookie settings