Maximum performance and flexibility in a streamlined design: the new KR CYBERTECH nano

With the KR CYBERTECH nano, KUKA presents a highly flexible multi-functional tool that deliverseven in the harshest environments. Low operating costs make the KUKA low payload robot particularly appealing for economically challenging production chains.

14 September 2020

Cost-effective robots, high flexibility

Whether as a handling robot, as a welding robot, for palletizing or for an adhesive application: the wide range of models and equipment of the new KR CYBERTECH nano from KUKA ensures almost unlimited application possibilities. In the low payload category between 6 and 10 kilograms, the cost-effective robot stands out for its speed and outstanding precision while keeping investment and maintenance costs low.
The KR CYBERTECH nano stands out for its streamlined design and versatility.
The main axes are protected to IP 65 against dust and water, the wrist axes even to IP 67.

Suitable for a wide range of applications – as a handling robot, welding robot and more

“With the new KR CYBERTECH nano, we are making industrial applications fit for the future,” says Markus Hollfelder-Asam, portfolio manager at KUKA. “Due to the flexible application potential combined with high performance, the investment pays off quickly and the KUKA robot in the low payload category immediately delivers top results in all areas.” The main reason for this is that the robot types are perfectly matched to their primary intended purpose.

The KUKA robot in the low payload category can be positioned at any angle

The new robot also excels in the handling of sensitive electronic components, being protected against uncontrolled electrostatic charging or discharging (ESD). Even humid or harsh environments are no problem for the KR CYBERTECH nano: the main axes are protected to IP 65 against dust and water, the wrist axes even to IP 67. Moreover, the KUKA robot in the low payload category can be installed in any position – on the floor, ceiling or wall – and at any angle.
The wide range of equipment of the new KR CYBERTECH nano ensures almost unlimited possibilities.

Identical footprint, the same connection patterns and full accessory compatibility with its predecessor make the changeover quick and easy.

Markus Hollfelder-Asam, Portfolio Manager at KUKA

Cost-effective robots optimized for maximum performance

The KR CYBERTECH nano is optimized for use with the new-generation KR C5 robot controller from KUKA in combination with the latest KUKA.SystemSoftware KSS 8.7. The integrated 600 V technology ensures high performance, while the finely tuned Motion Modes make the robot precise, fast and adaptable. Its high repeatability at any speed makes the KR CYBERTECH nano well suited for compact cells, complex tasks and challenging production chains. The further refined motion characteristics compared to the previous series guarantee precise continuous-path performance.
In conjunction with the new KR C5 robot controller, the KR CYBERTECH nano delivers maximum performance.
Cookie settings OK and discover KUKA

This website uses cookies (find out more) in order to offer you the best service online as well. If you simply continue to use our website, we will only use cookies required for technical purposes. If you click on “OK and discover KUKA”, you are also agreeing to the additional use of marketing cookies. You can select which cookies we use by clicking on “Cookie settings”.

Cookie settings