Select your location:

Country

Laser soldering

Laser soldering enables substance-to-substance bonds. The laser can be focused with high accuracy. This means that even the smallest soldered joints and sensitive electronic components can be connected. The technology is also frequently used in the automotive industry or in the electronics sector.


Laser soldering: the technology

Laser soldering is a non-contact process: the laser beam heats up the solder. This is then introduced to the process as a filler wire, which usually consists of copper or zinc alloys. The solder then melts and fills the joint gap. The melt fuses the two components.

Laser soldering is subdivided into two variants:

  1. Laser hard soldering, or laser brazing, with melting temperatures above 450 degrees Celsius:
    This joining technique uses diode lasers with higher power and is used primarily in the automotive industry.
  2. Soft laser soldering with melting temperatures below 450 degrees Celsius:
    This technique is commonly used in the manufacture of electronic components.

Automated laser soldering

As a KUKA customer, you have two options:

  • Automated and scalable production systems
  • Individually configured manufacturing cells

Parameters such as path velocity, laser power or optimum wire feed are second nature to us, and we offer various technology packages for different production scenarios.

Laser soldering in the process

What advantages does KUKA laser soldering offer?

  • Top performance

    • High process speed
    • Minimum heat input
    • Temperature control of the soldered joint
    • Low component distortion
  • Diversity

    • Soldering of sensitive and dissimilar components
    • Wide range of robots for applications in different industries and sectors
    • Robotic (cell) solutions with system partners
  • Know-how & service

    • Years of process expertise
    • Own gripper for soldering of the roof seam
    • Custom-tailored process solutions
  • Quality

    • Paintable seams, without reprocessing work
    • Fewer restrictions due to zinc coating
    • Possibility of seal welds
    • Harmonious component transitions at visible seams
    • Gap compatibility
    • No structural change
    • High strength of the workpieces

KR QUANTEC

With a payload of 120 to 240 kg, the versatile robot automates your laser soldering process.

White Paper: Welding aluminum? No problem! Score high now in production for electromobility.

Due to its ideal combination of strength and light weight, aluminum plays an important role in electromobility. In welding and joining processes, aluminum places high demands on the technologies used. With comprehensive process know-how and the right products, KUKA prepares you for the technological transformation towards electromobility. The battery box example shows how robots enable the production of aluminum components to the highest quality standards. 

Read about what is important for aluminum welding in the electromobility sector

Download White Paper

Do you want to optimize your laser soldering process?

We will create the right laser soldering process for you and together we will find the ideal solution for your specific requirements.

More information about technologies using lasers

With KUKA, laser applications mean automation, accuracy and significant process improvement.
  • Preview 1
  • Preview 2
  • Preview 3

Find more details about our laser technologies in the brochure.

Download here

This website uses cookies (find out more) in order to offer you the best service online as well. If you simply continue to use our website, we will only use cookies required for technical purposes. If you click on “OK and discover KUKA”, you are also agreeing to the additional use of marketing cookies. You can select which cookies we use by clicking on “Cookie settings”.

Cookie settings