Visit us at Booth W2-28 in West Hall and experience KUKA automation solutions first hand
Based on the theme of
"Sensitive Robots and Mobility Solutions for Adaptive Production
Systems", KUKA is showcasing various human-friendly
solutions such as a
sensitive robot LBR iiwa , a
LBR Med, the first robotic component worldwide to have been certified with a CB Report for integration into a medical product and an automatic
KUKA charging assistant carla _
connect for electric and plug-in hybrid vehicles. The new generation of the KUKA bestseller,
KR QUANTEC sets new standards through its quality, reliability, flexibility and cost-effectiveness.
Innovative, robot-based medical assistance functions
At iREX, KUKA will is presenting the wide range of potential medical applications of the
LBR Med. One
application example being demonstrated at the trade fair for this robot, which is designed for human-robot collaboration, is spinal surgery. Here, the robot is either guided manually to the area of the spine to be operated or it can automatically move to the desired position – using a suitable imaging system or a connection to an external camera. The LBR Med holds its defined position at the area to be treated and assists during the operation.
The next generation: the new KR QUANTEC features greater performance, precision and speed than ever before
The KR QUANTEC is the world’s first industrial robot to have digital Motion Modes. The software add-ons can be activated easily on the robot controller, optimizing the performance of the robot for important motion sequences. Depending on the work step, the robot can switch to and from between the individual Motion Modes.
Performance mode: impressively versatile and the right Motion Mode for the majority of tasks – from handling and spot welding to machining and loading/unloading.
Path mode: is used for continuous-path motion and increases the precision for both low and high path velocities – for example in adhesive bonding, measuring or laser applications.
Dynamic mode: the right choice when the objective is to reduce cycle times.
Hardware becomes software – thanks to the add-on digital plug-in Motion Modes