Angela Merkel Beata Szylo und Dr. Till Reuter auf der Hannover Messe 2017

Angela Merkel visits KUKA at Hannover Messe

KUKA CEO Dr. Till Reuter welcomed German Chancellor Angela Merkel und Polish Prime Minister Beata Szydlo at the KUKA booth at Hannover Messe 2017.

24 April 2017

As a memory he presented them an individual jigsaw puzzle from the Smart Factory - the biggest connected fair application in KUKA's history.

On the first day of Hannover Messe 2017 a fair round-trip had Angela Merkel and Beata Szydlo paying a visit to the KUKA booth. Aside from the Smart Factory, Dr. Till Reuter and CFO Peter Mohnen also showed them a particularly compact robot: the KR CYBERTECH nano.  A robot with extraordinary performance in the low payload class. Agile, flexible and equipped with a high reach, starring also in small spaces.

Jigsaw puzzle from the Smart Factory for Angela Merkel

As a souvenir for the visit at the KUKA booth, Dr. Till Reuter presented an individual jigsaw puzzle produced in the Smart Factory. The biggest connected fair application in KUKA's history produced both puzzles in batch size 1 right at the KUKA booth.

The theme for Angela Merkel showed her and Dr. Till Reuter during her visit to the KUKA production in Augsburg in 2015. Beata Szydlo received a puzzle with a robot jointing a German and a Polish flag.

Angela Merkel und Beata Szydlo besuchen den Stand der KUKA AG auf der Hannover Messe 2017
Fresh out of the Smart Factory: Dr. Till Reuter and Peter Mohnen present Angela Merkel and Beata Szydlo an individually produced jigsaw puzzle.

KUKA in Poland

„Serdecznie witamy!“ – Welcome – was the slogan on the big screen above the booth. The KUKA offices in Poland were founded 2008 in Katowice. With sales, service and its own KUKA College KUKA is offering the full portfolio in the country. In 2016, a second sales office was opened in Bydgoszcz to better serve northern Poland.

Cookie settings OK and discover KUKA

We use cookies to offer you the best service online, as well. More under Privacy Policy.

Cookie settings