Flexible automation of self-pierce riveting with KUKA ready2_rivet

KUKA has expanded its product portfolio: the new member of the ready2_use team is called ready2_rivet. The preconfigured automation package ready2_rivet is the ideal self-pierce riveting solution for body-in-white applications.

18 April 2018

Flexible and versatile self-pierce riveting

The self-pierce riveting solution for body-in-white (BiW) applications has been developed jointly with Böllhoff, one of the world’s leading manufacturers and suppliers of fasteners and assembly systems. “The combination is the key,” says Burkhard Stimmel from KUKA. “Using the KUKA robot and controller paired with the expertise in mechanical joining technology of our partner Böllhoff, we were able to develop an automated, flexible and turnkey solution for BiW applications.” Customers benefit from the low effort required to integrate the self-pierce riveting application and from its versatility.

Using the KUKA robot and controller paired with the expertise in mechanical joining technology of our partner Böllhoff, we were able to develop an automated, flexible and turnkey solution for BiW applications.

Burkhard Stimmel, Portfolio Manager, KUKA Automotive Division
KUKA ready2_rivet is the universal automation solution for all applications in the field of self-pierce riveting

Addition to the range of ready2_use packages

The different ready2_use packages are sector-specific, industry-proven and ready for immediate use – as the name suggests. “Application-oriented solutions that provide our customers with an advantage in global competition are best developed in cooperation with a system partner,” explains Burkhard Stimmel. “This enables us to provide our customers with products that offer real added value.” Ready2_rivet was developed together with Böllhoff. The Quantec series robot is from KUKA, as is the robot controller. Böllhoff provides the self-pierce riveting technology. The KUKA KR C4 robot controller convinces with its worldwide compatibility: it works reliably with different mains voltages and types, even in extreme cold, heat or humidity. It speaks 25 languages – including the major Asian ones – and meets all globally relevant ISO and US standards.

 

The KUKA smartPAD makes operator control easy and intuitive, even for inexperienced users. In this case, the KUKA smartPAD also serves to simplify operator control and supports the process control of the overall system. Böllhoff provides the application components. The expert for mechanical joining technology uses its tried-and-tested self-pierce riveting process for joints that are accessible from both sides. “Lightweight construction in the automotive industry demands modern joining technologies,” says Horst Wittop from Böllhoff. “With our process, we set the rivets in a single operation without drilling pilot holes. Together with KUKA, we were able to implement perfectly coordinated components.” Both companies contributed their industry know-how in the automotive sector and their respective expertise in robotic and joining technology to bring a competitive product – the ready2_rivet package – to market. 


With our process, we set the rivets in a single operation without drilling pilot holes. Together with KUKA, we were able to implement perfectly coordinated components.

Horst Wittop, Wilhelm Böllhoff GmbH & Co. KG

Ready2_rivet: setting rivets in the age of Industrie 4.0

Manufacturing in production shops is undergoing a transformation. The reason for this is the increasing international competition and changing market demand. Product life cycles are becoming shorter. This naturally also applies to the automotive sector. Changing model series require solutions that are flexible and quick to put into operation. Lightweight construction, the technology of the future for saving materials and energy, calls for specialist expertise. If, for example, aluminum and steel are to be joined, factors such as the respective strengths of the materials and their deformation characteristics play an important role. Ready2_rivet is the answer to these challenges. The self-pierce riveting application can be seamlessly integrated into the existing production environment and boosts productivity and efficiency. It remains versatile at all times and can be adapted to new requirements – in keeping with the philosophy of Industrie 4.0. 

 

Experience the ready2_rivet package in operation!

Discover all the interesting product details for KUKA ready2_rivet and experience the preconfigured automation package for all self-pierce riveting tasks in operation. Our self-pierce riveting technology experts will be happy to answer any detailed questions you may have. 

ready2_rivet product page
Cookie settings OK and discover KUKA

We use cookies to offer you the best service online, as well. More under Privacy Policy.

Cookie settings