KUKA at MEDICA 2019

How can robot-based medical technology improve treatment and therapy for patients? KUKA is presenting answers to this question at MEDICA, the world’s largest trade fair for the medical technology sector. A further highlight is the presentation of the KUKA Innovation Award. 

23 October 2019

Visit us at Booth A22 in Hall 10 and experience KUKA technology for the medical sector at first hand

At MEDICA – taking place in Düsseldorf from 18 to 21 November – KUKA will again be presenting various applications based on the LBR Med lightweight robot. One of the exhibits will be the SculpturaTM from Sensus Healthcare. The mobile, robot-based system has the potential to revolutionize radiotherapy as it is the only medical product which allows doctors to carry out pinpoint irradiation of tumors in the body during an operation. Thanks to the integrated and sensitive 7-axis LBR Med robot, SculpturaTM enables a precise, fast and localized dose to be administered without damaging surrounding tissue. 

Focus on Healthy Living: KUKA presents the Innovation Award

The theme of the 2019 KUKA Innovation Award is “Healthy Living”, focusing on medical robotics for the first time. An international jury of experts selected the five best concepts, which will be presented live at MEDICA and compete for the monetary prize of 20,000 euro. The spectrum ranges from robotic applications in the field of bowel cancer diagnostics to neurosurgery and the treatment of microfractures in the spine. The solutions are based on the LBR Med.

Experience KUKA at MEDICA 2019

Find out further details about our trade fair applications and speak with our KUKA experts for the medical sector on site.

Get your free admission ticket
Cookie settings OK and discover KUKA

We use cookies to offer you the best service online, as well. More under Privacy Policy.

Cookie settings