KUKA robot mills oversized plastic pipes

At Asset International in South Wales, a KUKA 120 R2700 extra HA robot, a KL 1500-3 T linear unit, and two KUKA MG 360 servomotors for the external rotational axis and the KUKA CNC controller relieve workers of strenuous milling tasks.

5 de septiembre de 2016

KUKA partner Eugen Riexinger GmbH & Co. KG has developed a fully integrated, automated solution for the milling of huge plastic pipes using KUKA KR QUANTEC robots

The KUKA KR QUANTEC series for payloads of up to 120 kilograms

The KUKA 120 R2700 extra HA robot from the KUKA KR QUANTEC series for payloads of up to 120 kilograms is designed for high-precision requirements such as milling and laser applications. At Asset International, it machines the large plastic pipe components with a specially designed high-speed milling spindle. Prior to machining, workers clamp the components to a multi-functional clamping table or a large, self-centering table controlled by the rotational axis. As a result of the barrier-free system, the robot, mounted on the KL 1500-3 T linear unit, can move directly to the plastic pipe to be machined and then flexibly carry out the job on the component as required. The solution was developed by integrator Eugen Riexinger GmbH & Co. KG in Bad Liebenzell.
The robot takes over the strenuous milling tasks on the oversized plastic pipes.

40 percent productivity boost and increased safety

“Thanks to the KUKA 120 R2700 extra HA robot, our employees are relieved of very strenuous manual work involving strong vibrations,” says Graham Bennett. “The solution has enabled us to increased productivity by more than 40 percent,” says Asset’s Operation Manager with pleasure. “Shorter production times have allowed us to boost capacity by more than 50 percent. At the same time, there has been a significant improvement in quality and precision,” he emphasizes.

Thanks to its modular design tailored to the customer’s requirements, the system can be adapted to the needs of Asset International at any time. The integrator is also very pleased with the result. “We are very proud to have designed the first system worldwide that can process such large plastic parts with this precision and speed – all the while increasing occupational safety,” emphasizes Manuel Kratz, head of the project at Riexinger. For this reason, the Bad Liebenzell-based company is sure that robot-based automation in the plastics processing sector will be seeing further growth.

Find out more about the KUKA KR QUANTEC series

Configuración de cookies Aceptar y descubrir KUKA

Este sitio web utiliza cookies (saber más) para ofrecerle, también en internet, el mejor servicio. Si continua usando nuestra página web, utilizamos únicamente las cookies necesarias técnicamente. Si hace clic en «Aceptar y descubrir KUKA», acepta también la utilización de cookies de marketing. Al hacer clic sobre «Configuración de cookies» puede seleccionar las cookies que utilizamos.

Configuración de cookies