KUKA wins major systems engineering contract from U.S. automotive manufacturer

The project comprises the design and installation of a highly flexible manufacturing system to produce body components for a range of vehicle variants.

22 de marzo de 2018

KUKA Systems has won a substantial systems engineering contract from a major U.S. automotive manufacturer. The project comprises the design and installation of a highly flexible manufacturing system to produce body components for a range of vehicle variants. The order volume lies in the high double-digit-million euro range and was booked in the fourth quarter of 2017. The start of production is scheduled for 2019.

At the North American plant, automated joining processes are to be integrated into the line for the front structure, underbody and body framing of the vehicle. The line is to include the KUKA KS Framer, which can produce up to six different models.

“We are proud that we have once again been able to convince our customer with our high-tech products. At the same time, this order underscores the out-standing partnership between our two companies,” explains Dr. Till Reuter, CEO of KUKA AG.

 

Descargar mensaje de noticias

NewsDownloadButtonLabel
Configuración de cookies Aceptar y descubrir KUKA

Este sitio web utiliza cookies (saber más) para ofrecerle, también en internet, el mejor servicio. Si continua usando nuestra página web, utilizamos únicamente las cookies necesarias técnicamente. Si hace clic en «Aceptar y descubrir KUKA», acepta también la utilización de cookies de marketing. Al hacer clic sobre «Configuración de cookies» puede seleccionar las cookies que utilizamos.

Configuración de cookies