KUKA wins major systems engineering contract from U.S. automotive manufacturer

The project comprises the design and installation of a highly flexible manufacturing system to produce body components for a range of vehicle variants.

22 mars 2018

KUKA Systems has won a substantial systems engineering contract from a major U.S. automotive manufacturer. The project comprises the design and installation of a highly flexible manufacturing system to produce body components for a range of vehicle variants. The order volume lies in the high double-digit-million euro range and was booked in the fourth quarter of 2017. The start of production is scheduled for 2019.

At the North American plant, automated joining processes are to be integrated into the line for the front structure, underbody and body framing of the vehicle. The line is to include the KUKA KS Framer, which can produce up to six different models.

“We are proud that we have once again been able to convince our customer with our high-tech products. At the same time, this order underscores the out-standing partnership between our two companies,” explains Dr. Till Reuter, CEO of KUKA AG.

 

Télécharger les nouvelles

NewsDownloadButtonLabel
Réglages des cookies OK et découvrir KUKA

Ce site internet utilise des cookies (en savoir plus) afin de vous proposer le meilleur service en ligne. Si vous continuez à utiliser notre site internet, nous n’aurons recours qu’aux cookies techniquement nécessaires. Si vous cliquez sur « OK et découvrir KUKA », vous acceptez en plus l’utilisation de cookies de marketing. En cliquant sur « Paramètres des cookies », vous pouvez sélectionner le type de cookies employé.

Réglages des cookies