Iniziare a lavorare con iiQKA

The future KUKA operating system will mark the beginning of a new era in robotics

As easy to use as a smartphone: At Hannover Messe, KUKA presents the first look at its new operating system, iiQKA.OS, which will significantly simplify robot use.

12 aprile 2021

On the way to a new era of intuitive, fast and powerful automation for all, KUKA previews the first elements of the future operating system, iiQKA.OS, at the digital Hannover Messe. The new operating system will form the base of an entire ecosystem, providing access to a powerful selection of components, programs, apps, services and equipment that are easy to install, operate and use to enhance the system. This iiQKA Ecosystem based on iiQKA.OS will make it possible for newcomers to implement automation without specialized training, while greatly improving and simplifying the process for experts.

Making robot-based automation easily available to all

“Automation is one of the megatrends of our time. That is why KUKA aims to make robot-based automation available to everyone as part of its ‘Mission 2030’,” says Kristina Wagner, Vice President Corporate Research & Director Robot X-perience Program. This is where the new operating system iiQKA.OS supported by the iiQKA Ecosystem comes into play: It is based on a modern and modular software architecture with usability and intuitive, user-friendly features built in across the user journey – and will thus offer a quick introduction to robotics for beginners and a significant improvement in automation for experienced users. 

Powerful package of software, services and an easy-to-use KUKA robot

Overall system of hardware and software is crucial

Software is more important than ever for the user-friendliness of an entire robot system. This requires an operating system that is intuitive to use and offers access to an ecosystem of components, programs, apps, services and accessories – such as will come with iiQKA.OS. The sensitive cobot LBR iisy will be the first of its kind to run exclusively on the new operating system supported by the iiQKA Ecosystem – in combination with the KR C5 micro robot controller and the new smartPAD pro operator device. KUKA's aim is not only to make robotics more accessible to newcomers, but also to further develop its existing customer base. Over the next years, the goal is for every KUKA product to be equipped with the new iiQKA.OS and iiQKA Ecosystem – it is a long-term development project in which the first steps have now been made.
The cobot of a new era of automation: KUKA's LBR iisy

Network of partners and developers

Starting with selected partners, the iiQKA Ecosystem will grow to become an open network of partners and developers who provide hardware and software  for example, a selection of grippers or other end-of-arm-tooling, camera systems for visual recognition, safety sensor technology or application-specific programs. This is exemplified by KUKA’s first iiQKA Ecosystem Keystone Partners: SCHUNK, SICK and Roboception. Open and standardized interfaces play an important role here, enabling partners and developers to provide such hardware and software extensions in a simple way, harnessing the power of the iiQKA.OS usability platform. End customers and integrators benefit from this by quickly and easily finding the right combination of KUKA products and ecosystem provider add-ons for their particular application. Thus, in the coming years, the ecosystem will offer functionalities and services that make the KUKA portfolio more flexible and powerful, able to adapt and scale as quickly as the market demands. 

Intelligent solutions for more user-friendliness

Built on a Linux kernel, the entire architecture of the new OS is designed for rapid development and maximum user-friendliness: iiQKA.OS will provide updates and upgrades quickly, so that more functions will be added over time. The new OS will also support the existing KUKA Robot Language (KRL). This will allow existing customers who have expertise with KUKA.SystemSoftware to migrate smoothly to iiQKA.OS in the coming years and continue to use workflows and codes.  
Impostazioni cookie OK e scopri KUKA

Questo sito web utilizza i cookie (per saperne di più) per offrivi l’assistenza migliore anche online. Se si continua a navigare sul nostro sito web, utilizziamo solo i cookie necessari dal punto di vista tecnico. Cliccando su ""OK e scopri KUKA"", si accetta anche l'utilizzo di cookie di marketing. Con un clic su ""Impostazioni cookie"" è possibile selezionare quali cookie utilizziamo.

Impostazioni cookie