Experience matrix production live in the KUKA SmartProduction Center

Experience today the production of tomorrow at the KUKA site in Augsburg. In the KUKA SmartProduction Center, the versatile and flexible matrix solution becomes reality. Different products can be manufactured on the same system – customized production is possible.


Experience today the production of tomorrow

KUKA is inviting customers and partners to witness the moment in which a vision becomes reality. The versatile and flexible matrix production solution is being put into operation in the SmartProduction Center” at the Augsburg site. The smart system is centered on the new KUKA software package KUKA SmartProduction_control. It has all the necessary information and controls the processes: from the robot to the automated guided vehicles (AGVs).

Our intelligent software has an overview. It knows where the moving AGVs are located, which component the AGV needs to deliver to the robot, and quickly prepares a conversion.

Dr. Andreas Bauer, software architect in the KUKA Automotive division

A smart solution is needed.

Increasing type variety, more frequent changes of model, quantity fluctuations: the new market conditions require a suitable and competitive production solution. “We can offer this with matrix production,” says Dr. Andreas Bauer, software architect in the KUKA Automotive division.

How can I produce different parts on a single system? How can production be stepped up at short notice? How can I carry out a change of type within a short period of time on the same system?

A smart solution is needed. That is why KUKA has developed matrix production: together with the automated guided vehicles (AGVs), the KUKA SmartProduction_control software package, which is based on artificial intelligence (AI) technologies, ensures, among other things, that production is flexible and versatile. A product-neutral production facility requires the separation of production and intralogistics. The decoupling of intralogistics from production is another key advantage of smart matrix production. Controlled by KUKA SmartProduction_control, the AGVs fetch tools from a tool store and then transport them in to the production cells that are to be equipped. At the same time, the AGVs move to the centralized material warehouse, which is decoupled from production, in order to transfer the centrally-stored components required for the production process into the cells. Matrix production can thus become a decisive competitive advantage compared with rigidly linked production concepts.

With the configurable production cells, combined with the freely programmable intralogistics and our new KUKA SmartProduction_control software package, we are able to provide our customers with everything they need for flexible and versatile production.

Dr. Johann Härtl, Head of Competence Center of the KUKA Automotive division

Smart manufacturing with KUKA matrix production 

In order to demonstrate the principle of matrix production to our customers, a pilot system has been built and is being put into operation with the opening ceremony on 20 March 2018. Here customers can experience the matrix concept at first hand. It is based on standardized production cells. All cells are equipped with product-neutral basic functions and can be simply expanded with product-specific tools depending on the level of orders and batch sizes.

Fully automated component and tool transportation with AGVs

Fully automated intralogistics with AGVs

Equipping the production cells and transporting the components: everything is carried out fully automatically by AGVs. The individual robots pick up the components supplied to them by the AGVs and join them using the corresponding technology. In the test cell, car doors and wheel arches for different OEMs are manufactured on the same system: conversion is carried out in a short space of time. The intralogistics structure consists of AGVs and a warehouse in which the components are provided. The dedicated tools, on the other hand, are located in the tool store. A software package ensures that the automatic process runs smoothly: KUKA SmartProduction_control is familiar with all activities at all times, proactively controls them, and thus has an overview of the motions of the AGVs, their battery charge and the current status of the production cells. 

Advantages of the matrix production concept at a glance

What is the best way to explain theoretical considerations? By implementing them in reality. That is precisely what we have done with the matrix production concept. In the SmartProduction Center, customers can see for themselves the impressive advantages of the matrix solution. Manufacturing different products on the same system, enabling the production facility to breathe, customized production: all of these things are possible with matrix production.

The versatility of the system is perhaps the most decisive criterion. In this way, we can meet customer requirements. We are at the forefront of developments in this field.

Larry Drake, CEO KUKA Automotive division

The system is converted within a short time. Compared with previous rigidly linked production, the production facility requires the same space, but can be optimally distributed within that space. Due to the centralized logistics, less personnel is directly tied to the system and to the logistics. Furthermore, intermediate storage areas and material provision at the system are dispensed with. Matrix production is therefore also more cost-effective. Why? The entire value chain is networked, thereby enabling holistic optimization of the system.

Conclusion: Production becomes more flexible, competitiveness is increased and cost-effectiveness is improved.