McLaren Summer Boutique

At the McLaren Summer Boutique in Zurich, KUKA, in collaboration with McLaren Zurich and the Association for Robots in Architecture, is presenting an art project based on the latest generation of industrial robots. The installation symbolizes the fusion of first-class vehicle design with state-of-the-art automation technology and maximum precision.

2018年6月12日

Unbeaten for over 50 years

With 50 years of racing success behind them, McLaren has created some of the most legendary and exciting road vehicles the world has ever seen. KUKA has also been building industrial robots for almost 50 years and has reached the pole position by continuously optimizing its products. KUKA is now the world's number 1 in the field of robot-based automation in the automotive industry.

KUKA "Quantec KR 180 R2500 extra" in black with the McLaren "570S Spider" in orange.

弊社はオンラインでも最善のサービスを提供するためにCookieを利用しています。詳細はこちらをご覧ください

同意