KUKA receives a frame contract for 3,000 robots from Daimler AG

Augsburg, March 10, 2011

2011년 3월 10일

Daimler AG has decided to purchase KUKA's new QUANTEC generation of robots, which uses the new KR C4 robot control system. KUKA was able to win a frame contract for the supply of 3,000 industrial robots.

The new industrial robots cut energy consumption by up to 30 percent, without negatively impacting performance. The design features have also resulted in better dynamic performance, which ultimately is reflected in significantly shorter cycle times. In other words: lower energy consumption, smaller footprint but considerably higher production output. In addition, the number of model types has been streamlined and aligned with customer needs.

The robot's new KR C4 control system is as impressive as its advantageous mechanical features. The latest technical advances in IT technology were applied to replace a large part of the proprietary hardware with smart software solutions. This eliminates the limitations of many conventional interfaces, enabling users to now apply the robots in completely new scenarios and integrate new safety concepts.

"We are pleased that a customer as technologically demanding as Daimler opted for our new robot generation," said KUKA AG CEO Dr. Till Reuter. "This underscores our technical strength in the robot market and our market leadership in the automotive business."

쿠키 설정 OK 및 KUKA 알아보기

이 웹사이트에서는 온라인에서도 최고의 서비스를 제공하기 위해 쿠키(상세 정보)를 사용하고 있습니다. 이 웹사이트를 계속 이용하시는 경우 기술적으로 필요한 쿠키만이 사용됩니다. “OK 및 KUKA 알아보기”를 클릭하시면 귀하는 추가적으로 마케팅 쿠키의 사용에 동의하시게 됩니다. “쿠키 설정” 클릭 한 번으로 귀하가 허용하실 쿠키를 선택할 수 있습니다.

쿠키 설정