Major order from Ford

KUKA receives major order from Ford in Spain to automate a body-in-white line

2011년 10월 20일

KUKA Systems has received a major order from Ford in Europe. Under the terms of the contract, the division will automate a body-in-white line for the successor to the Ford KUGA at the company’s plant in Valencia, Spain.

As part of this order, KUKA Systems will deliver manufacturing systems for components such as doors, fenders, engine hoods and tailgates. The parts will be welded, glued or folded at upstream manufacturing cells and then automatically sent to the body-in-white assembly line for the new Ford KUGA, thereby improving the line’s efficiency. After the upgrade has been completed in the first half of 2012, the line will be capable of producing a considerably higher number of vehicles. The value of the order, which was booked in the third and fourth quarters of 2011, is in the lower double-digit million euro range.

Especially impressive is the fact that the systems and tools are being installed without shutting down the existing line. "This technically challenging project order from a long-standing and important automotive customer demonstrates that KUKA Systems earns high marks for quality,” said KUKA AG’s CEO Dr. Till Reuter.

쿠키 설정 OK 및 KUKA 알아보기

이 웹사이트에서는 온라인에서도 최고의 서비스를 제공하기 위해 쿠키(상세 정보)를 사용하고 있습니다. 이 웹사이트를 계속 이용하시는 경우 기술적으로 필요한 쿠키만이 사용됩니다. “OK 및 KUKA 알아보기”를 클릭하시면 귀하는 추가적으로 마케팅 쿠키의 사용에 동의하시게 됩니다. “쿠키 설정” 클릭 한 번으로 귀하가 허용하실 쿠키를 선택할 수 있습니다.

쿠키 설정