KUKA wins major order to build car body and parts assembly systems in China

KUKA Systems GmbH received a major order in the second quarter of 2012 to construct manufacturing lines for new car body and parts assembly systems in China

2012년 7월 30일

 A premium German carmaker awarded the order to furnish equipment for a Chinese manufacturing facility to technology leader KUKA Systems' local representative in the country. The order is valued in the lower double-digit millions Range (EUR). The project comprises a total of nine lines, which will be used to build car body subassemblies such as front and rear doors, fenders, engine hoods and tailgates. Also included in the order are an assembly and finishing line.

"Expanding our market share in China is still one of our key priorities. With orders like these, we can continue to successfully implement our strategy and achieve our target objectives," says Dr. Till Reuter, CEO of KUKA AG. KUKA Systems GmbH in Augsburg will help the local subsidiary in China with the project management, design, assembly and startup for the plant. The automated system includes 105 KUKA KR Quantec industrial robots, which will perform tasks such as spot welding, clinching, folding, gluing and subassembly handling.

쿠키 설정 OK 및 KUKA 알아보기

이 웹사이트에서는 온라인에서도 최고의 서비스를 제공하기 위해 쿠키(상세 정보)를 사용하고 있습니다. 이 웹사이트를 계속 이용하시는 경우 기술적으로 필요한 쿠키만이 사용됩니다. “OK 및 KUKA 알아보기”를 클릭하시면 귀하는 추가적으로 마케팅 쿠키의 사용에 동의하시게 됩니다. “쿠키 설정” 클릭 한 번으로 귀하가 허용하실 쿠키를 선택할 수 있습니다.

쿠키 설정