KUKA robot saws wooden stools

The unadulterated brand experience: That is the goal of the BMW Brand Store in Brussels. A KUKA robot, equipped with a chainsaw, is the highlight attraction of the current exhibit.

2014년 11월 3일

At the heart of the exhibit is the presentation of the new 2 Series Active Tourer vehicle. A BMW model that, first and foremost, is aimed at two groups: families and nature lovers. The BMW Brand Store in Brussels is, however, not a retail store. Situated prominently in the city center, the goal here is not sales, but experiencing the BMW brand.

To this end, the exhibit as well as the design change every three months. For the presentation of the 2 Series Active Tourer, the focus was placed on outdoor scenes characterized by nature and recreational experiences. The target audience of this current BMW storyline: persons leading an active lifestyle who value outdoor activities and a sense of community.

KUKA robot moved into live action display 

Nestled in outdoor scenery, a KUKA robot moved into the live action display area in September. Equipped with a chainsaw, the goal was to combine classic outdoors activities with innovation and technology. New target groups should be reached and through the extravagant installations valuable customers are intended to be pulled into the store. The robot catches the eye as people walk past the display window. Particularly when the robot is in action. Positioned inside a glass case, it saws two three-legged stools from a single log. It requires about 15 minutes completing these two pieces of furniture.

The feeling of the outdoors in the BMW brand store

A log, a chainsaw and a robot fit into the current store design very nicely. Real trees have been installed in the store. The natural look is rounded off with many small wooden cases that function as presentation boxes or planter boxes. The wood used comes from the sustainable forests of the Echtwald company and will be reused after the demonstration. The robot performance itself was developed by Tom Pawlofsky within his teaching activity at the Karlsruhe College of Arts and Design.

The produced stool named “7xstool” was developed in cooperation with Tibor Weissmahr. The robot has already completed more than 100 stools since the start of the exhibit. The robot will be in action in the BMW Brand Store in Brussels until the end of November. The furniture completed by then will be reused. They will be placed as props in the winter exhibit starting at the end of November at BMW Welt in Munich.

쿠키 설정 OK 및 KUKA 알아보기

이 웹사이트에서는 온라인에서도 최고의 서비스를 제공하기 위해 쿠키(상세 정보)를 사용하고 있습니다. 이 웹사이트를 계속 이용하시는 경우 기술적으로 필요한 쿠키만이 사용됩니다. “OK 및 KUKA 알아보기”를 클릭하시면 귀하는 추가적으로 마케팅 쿠키의 사용에 동의하시게 됩니다. “쿠키 설정” 클릭 한 번으로 귀하가 허용하실 쿠키를 선택할 수 있습니다.

쿠키 설정