Simple integration of robots into the machine environment

The development of robot software KUKA.PLC mxAutomation

2015년 11월 19일

With the software KUKA.PLC mxAutomation, KUKA Roboter GmbH has developed a solution that enables simple integration of the robot into the machine controller.

Operators do not need to have specific robotics knowledge and can work in their usual programming and operator control environment. The robot is very easily integrated into the machine environment.

Through the further development of KUKA.PLC mxAutomation 2.1 software, now even more partners can easily incorporate KUKA robots into their machine environments. In addition to supporting the well-known partners Siemens, CoDeSys, AllenBradley and LabView, the software tool now also supports Beckhoff, Schneider Electric, B&R and the Siemens controllers TIA Portal (SIMATIC) and SIMOTION.

The new partners will be demonstrating the simple integration of the robot into the machine environment at their trade fair booths at SPS/IPC Drives in Nuremberg.

KUKA.PLC mxAutomation connects the robot with the machine control.
쿠키 설정 OK 및 KUKA 알아보기

이 웹사이트에서는 온라인에서도 최고의 서비스를 제공하기 위해 쿠키(상세 정보)를 사용하고 있습니다. 이 웹사이트를 계속 이용하시는 경우 기술적으로 필요한 쿠키만이 사용됩니다. “OK 및 KUKA 알아보기”를 클릭하시면 귀하는 추가적으로 마케팅 쿠키의 사용에 동의하시게 됩니다. “쿠키 설정” 클릭 한 번으로 귀하가 허용하실 쿠키를 선택할 수 있습니다.

쿠키 설정