KUKA shows innovation projects at the IROS research trade fair

In cooperation with the Hong Kong Applied Science and Technology Research Institute, KUKA is showing how new technologies help minimize complexity, costs and time in production at this year’s IROS in Macau.

2019년 10월 16일

The application at the International Conference on Intelligent Robots and Systems shows a robot welding system on a workpiece. First, the user defines the welding path in the virtual world using a 3D model of the workpiece. Thereafter, everything runs automatically: a camera detects the workpiece and determines its pose in space and in relation to the robot. For this, various algorithms come into play in order to estimate the position – some using artificial neural networks – and to plan the motion. The robot then executes the determined process path. A laser pointer helps to visualize the welding process.

Digital and physical twin.

Faster, simpler and less expensive thanks to digital images

The combination of simulation in the virtual world and camera-based automatic calibration in the real world enable the system to adapt quickly to new workpieces and potential variations. Processes can also be checked and optimized in the simulation. Digital twins help to minimize the complexity of the design and thus to reduce cost and time.

A classic carnival game re-imagined

In a very special version of the popular reaction game “Whac-A-Mole”, visitors also have the chance to compete against a KR 3 Agilus robot at the KUKA booth. Small toy robots appear at random in holes in a board. Visitors must use a rubber mallet to strike them back into their holes. Who can react faster – the human or the robot?

About IROS 2019

The International Conference on Intelligent Robots and Systems is one of the most important robotics conferences worldwide. This year, a new record number of about 4000 international experts are expected to come together to exchange views on the latest inno-vations and technical developments in workshops, forums, discussions and the accompa-nying robot exhibition. In addition to the exhibition, KUKA will be actively involved in fo-rums and workshops , including the CEO forum, the Industrial Forum and the workshop on the topic of “Intelligent Robotics Research” to encourage the exchange of ideas between industry and research. The conference is sponsored in part by the IEEE (Institute of Electrical and Electronics Engineers), as well as by other associations and societies.

 

Learn more about IROS 2019.

 

뉴스 보도 다운로드

PDF 다운로드
쿠키 설정 OK 및 KUKA 알아보기

이 웹사이트에서는 온라인에서도 최고의 서비스를 제공하기 위해 쿠키(상세 정보)를 사용하고 있습니다. 이 웹사이트를 계속 이용하시는 경우 기술적으로 필요한 쿠키만이 사용됩니다. “OK 및 KUKA 알아보기”를 클릭하시면 귀하는 추가적으로 마케팅 쿠키의 사용에 동의하시게 됩니다. “쿠키 설정” 클릭 한 번으로 귀하가 허용하실 쿠키를 선택할 수 있습니다.

쿠키 설정