위치를 선택하십시오:

국가

Welcome to Alihankinta!

KUKA Nordic is coming to Tampere with several news


Alihankinta Subcontracting fair is back. On the 21th of September, the fair will open its doors and KUKA Nordic will be on site, booth E 219. - I look forward meeting our Finnish customers and discussing automation and developments in robotics, says Kim Reeslev, Sales Manager Nordic and Baltics at KUKA Nordic. KUKA brings the new KR IONTEC, new KR C5 controller and its latest SCARA robot. There will be presentations of the robots directly on the exhibition floor. - We will make simpler demonstrations, and our product specialists are there and can answer questions, says Kim Reeslev.

KR IONTEC, shown at Alihankinta, is a flexible robot for load carriers between 20 and 70 kilos. It has a waterproof and dustproof central hand and the engine is protected. KR IONTEC can also be mounted in any position. - A very flexible robot, which also has a very competitive price, says Kim. The control unit KR C5 has several interesting features. The device has a compact format that saves space. It can interact seamlessly in complicated environments where several applications coexist. The device is also compatible with virtually all of the earlier version KR C4's applications.

When it comes to KUKA's latest SCARA robot, which will also be shown at Alihankinta, it is an ultra-compact robot, with a very short cycling time that can handle weights up to six kilos. The robot is reliable and durable and requires only a minimum of maintenance and has a very good Total Cost of Ownership.
According to Kimmo Kymäläinen, Alihankinta is a good forum to meet and discuss solutions with customers, contacts and other interested parties. - There are usually very good discussions and questions that we can take home, it will be very fun to get out into the exhibition environment again.  

Welcome to Alihankinta, visit us in Booth E 219

이 웹사이트에서는 온라인에서도 최고의 서비스를 제공하기 위해 쿠키(상세 정보)를 사용하고 있습니다. 이 웹사이트를 계속 이용하시는 경우 기술적으로 필요한 쿠키만이 사용됩니다. “OK 및 KUKA 알아보기”를 클릭하시면 귀하는 추가적으로 마케팅 쿠키의 사용에 동의하시게 됩니다. “쿠키 설정” 클릭 한 번으로 귀하가 허용하실 쿠키를 선택할 수 있습니다.

쿠키 설정