QUANTEC series – a wide range of variety
KUKA Roboter GmbH is presenting its new KR QUANTEC robot series – the successor to the bestselling comp and 2000 series.
15 czerwca 2010
Design
The robots of the KR QUANTEC series feature the customarily robust KUKA quality. The series has been designed with implementation of a concept based on common parts with just four motor and gear unit variants. All models have the same hole pattern for the mounting base, the same as that for the previous series, and an identical tool flange on the wrist. The KR QUANTEC series is thus 100% compatible with existing cell layouts based on the Series 2000. The design of the KR QUANTEC series is characterized by minimized disruptive contours and a compact wrist for accessibility even in confined spaces.The Quantec series model range consists of the four following product lines:
- KR QUANTEC ultra for payloads up to 300 kg
- KR QUANTEC prime for payloads up to 240 kg in spot welding, etc.
- KR QUANTEC extra as a versatile all-round robot for payloads up to 210 kg
- KR QUANTEC pro up to 120 kg
About the KUKA Robot Group
The KUKA Robot Group employs about 2000 people worldwide. Of these, some 1100 are employed in Germany. In 2009, sales totaled 330.5 million euro. 25 subsidiaries provide a presence in the major markets of Europe, America and Asia.