KUKA wins major systems engineering contract from U.S. automotive manufacturer

The project comprises the design and installation of a highly flexible manufacturing system to produce body components for a range of vehicle variants.

22 martie 2018

KUKA Systems has won a substantial systems engineering contract from a major U.S. automotive manufacturer. The project comprises the design and installation of a highly flexible manufacturing system to produce body components for a range of vehicle variants. The order volume lies in the high double-digit-million euro range and was booked in the fourth quarter of 2017. The start of production is scheduled for 2019.

At the North American plant, automated joining processes are to be integrated into the line for the front structure, underbody and body framing of the vehicle. The line is to include the KUKA KS Framer, which can produce up to six different models.

“We are proud that we have once again been able to convince our customer with our high-tech products. At the same time, this order underscores the out-standing partnership between our two companies,” explains Dr. Till Reuter, CEO of KUKA AG.

 

Descărcați știri

Descărcați PDF
Setări module cookie OK și descoperire KUKA

Această pagină web folosește module cookie (mai multe informații) pentru a vă putea oferi cele mai bune servicii și în mediul online. Dacă utilizați în continuare pagina noastră web, utilizăm numai module cookie necesare din punct de vedere tehnic. Dacă faceți clic pe „OK și descoperire KUKA”, sunteți de acord cu utilizarea modulelor cookie pentru marketing. Prin clic pe „Setări module cookie” puteți selecta modulele cookie pe care le utilizăm.

Setări module cookie