KUKA supplies battery production system for electric vehicles

KUKA Industries has received an order from a leading European manufacturer in the automotive industry to supply a further battery production system. The order value lies in the mid-double-digit million euro range and was booked in the second quarter of 2017. Start of production is planned for mid-2019.

den 2 augusti 2017

KUKA Industries has planned and set up the production system for the manufacture of battery modules and high-voltage batteries for use in electric vehicles. This involves individual battery cells being processed into modules and custom-tailored battery systems. The system to be delivered is based on KUKA standard cells, has a high level of automation and a modular design, which allows for the integration of additional process modules.

“The demands to be met in this sector are very high. In addition to reproducible quality of the highest level, vehicle manufacturers require a scalable automation solution that allows them to adapt to the growing demand, particularly in the production of battery modules,” explains Alwin Berninger, CEO of KUKA Industries GmbH.

“E-mobility is an opportunity for KUKA. By collaborating with our customers, we are in a position to press ahead with the electrification of the automotive industry. This order underscores the strength of our range of products and services,” emphasizes Dr. Till Reuter, CEO of KUKA AG.

Hämta nyhetsmeddelande

Vi använder kakor för att kunna erbjuda dig bästa möjliga service även online. Här finns mer information.

OK