KUKA shows innovation projects at the IROS research trade fair

In cooperation with the Hong Kong Applied Science and Technology Research Institute, KUKA is showing how new technologies help minimize complexity, costs and time in production at this year’s IROS in Macau.

16 ตุลาคม 2562

The application at the International Conference on Intelligent Robots and Systems shows a robot welding system on a workpiece. First, the user defines the welding path in the virtual world using a 3D model of the workpiece. Thereafter, everything runs automatically: a camera detects the workpiece and determines its pose in space and in relation to the robot. For this, various algorithms come into play in order to estimate the position – some using artificial neural networks – and to plan the motion. The robot then executes the determined process path. A laser pointer helps to visualize the welding process.

Digital and physical twin.

Faster, simpler and less expensive thanks to digital images

The combination of simulation in the virtual world and camera-based automatic calibration in the real world enable the system to adapt quickly to new workpieces and potential variations. Processes can also be checked and optimized in the simulation. Digital twins help to minimize the complexity of the design and thus to reduce cost and time.

A classic carnival game re-imagined

In a very special version of the popular reaction game “Whac-A-Mole”, visitors also have the chance to compete against a KR 3 Agilus robot at the KUKA booth. Small toy robots appear at random in holes in a board. Visitors must use a rubber mallet to strike them back into their holes. Who can react faster – the human or the robot?

About IROS 2019

The International Conference on Intelligent Robots and Systems is one of the most important robotics conferences worldwide. This year, a new record number of about 4000 international experts are expected to come together to exchange views on the latest inno-vations and technical developments in workshops, forums, discussions and the accompa-nying robot exhibition. In addition to the exhibition, KUKA will be actively involved in fo-rums and workshops , including the CEO forum, the Industrial Forum and the workshop on the topic of “Intelligent Robotics Research” to encourage the exchange of ideas between industry and research. The conference is sponsored in part by the IEEE (Institute of Electrical and Electronics Engineers), as well as by other associations and societies.

 

Learn more about IROS 2019.

 

ดาวน์โหลดจดหมายข่าว

ดาวน์โหลดเอกสาร PDF
การตั้งค่าคุ้กกี้ ตกลงและค้นพบ KUKA

"เว็บไซต์นี้มีการใช้ข้อมูลคุกกี้ (รายละเอียดเพิ่มเติม) เพื่อมอบประสบการณ์การบริการที่ดีที่สุดแก่คุณ หากคุณต้องการใช้เว็บไซต์ของเราต่อ เราจะใช้ข้อมูลคุกกี้ที่จำเป็นทางเทคนิคเท่านั้น หากคุณคลิก “ตกลงและค้นพบ KUKA” จะถือว่าคุณยอมรับให้ใช้ข้อมูลคุกกี้เพื่อประโยชน์ทางการตลาด คุณสามารถเลือกได้ว่าจะให้เราใช้ข้อมูลคุกกี้ประเภทใดด้วยการคลิก “การตั้งค่าคุกกี้”

การตั้งค่าคุ้กกี้