KUKA and Formula E

KUKA is partnering with the Audi Sport ABT Schaeffler team in the international motor sport series for electric cars, the FIA Formula E.

The Formula E racing calendar – 2019/2020

There will be a total of 14 races in the 2019/2020 season. They will be held in twelve major cities on five different continents. Here you will find an overview of the races that have already been run, the current races and future races. Daniel Abt and Lucas di Grassi from the Audi Sport ABT Schaeffler team will be challenging the world tour with their Audi e-tron FE06.

  • Diriyah

    November 22 & 23, 2019

    Race report
  • Santiago de Chile

    January 18, 2020

    Race report
  • Mexico City

    February 15, 2020

    Preview
  • Marrakesh

    February 29, 2020

    Preview
  • Sanya

    March 21, 2020

    Preview
  • Rome

    April 04, 2020

    Preview
  • Paris

    April 18, 2020

    Preview
  • Seoul

    May 03, 2020

    Preview
  • Jakarta

    June 06, 2020

    Preview
  • Berlin

    June 21, 2020

  • New York

    July 11, 2020

  • London

    July 25 & 26, 2020

Season 2019/20

Formula E started 2020 with a spectacular race in Santiago de Chile. Lucas di Grassi thrilled the South American fans with a forward charge from 22nd place on the grid to seventh place.

Formula E – exciting and innovative

Formula E, which was launched in September 2014, is the first exclusively electrical racing series and has managed to establish itself as an appealing motor sport event for a wide audience in only a short space of time and to inspire the best drivers, teams and manufacturers from around the world.

The racing series provides a competitive environment for the automotive industry in terms of promoting the development of electric cars. Audi's e-tron FE-06 is a good example of a racing car that has been developed into a standard vehicle. The races are held around the globe in the city centers of major cities. In this way, electromobility is showcased where it will be utilized in the future: in the urban environment.

What's more, fans of the racing series are able to make an impact on the races in a completely new way: they can give their favorite driver around 70 hp of additional power for a few seconds using the FanBoost. Unparalleled!

Formula E is perfectly suited to our competence in the areas automotive, eMobility and battery sectors. This is how KUKA has supported the Audi Sport ABT Schaeffler team since March 2017 as a partner and sponsor; the two companies having the common aspiration to give their best at all times: Peak performance.

FanBoost

The FanBoost in Formula E is unparalleled in motor sport. It allows spectators and fans to play an active role in the outcome of the race by enabling them to vote for their favorite driver and award them with extra power for the race.

The five drivers with the most votes receive 100 kJ of additional energy each. This additional energy can be used in the second half of the race in a 5-second window. During this window, the power of the racing car increases briefly from 200 kW (272 hp) to 250 kW (340 hp).

Voting begins six days prior to an E-Prix on a Monday at 5:30 p.m. local time and closes 15 minutes after the race has begun. Once the voting window has elapsed, Formula E announces the results during the live broadcast of the race.

How does voting take place?

You can vote on the official Formula E FanBoost website and by using a hashtag on the short message service Twitter:

 

#FANBOOST #DanielAbt

#FANBOOST #LucasdiGrassi

Formula E is the only racing format that allows fans to influence the outcome of the race.

Making the difference in Formula E race cars.

The car essentially consists of two main pieces. – One is the same for every manufacturer. That’s the chassis and also the battery. And then for us, in Audi, all of the development we do is on the electric motor, gear box, the rear suspension. So effectively the electric drivetrain – The power delivery. And there we’re now working on several items of performance: One is that we always want to reduce the weight and size. That allows a better exhilaration, but also less mas to move. So it’s better for the energy management.

Helmut, Systemingenieur, Team Audi Sport ABT Schaeffle
การตั้งค่าคุ้กกี้ ตกลงและค้นพบ KUKA

"เว็บไซต์นี้มีการใช้ข้อมูลคุกกี้ (รายละเอียดเพิ่มเติม) เพื่อมอบประสบการณ์การบริการที่ดีที่สุดแก่คุณ หากคุณต้องการใช้เว็บไซต์ของเราต่อ เราจะใช้ข้อมูลคุกกี้ที่จำเป็นทางเทคนิคเท่านั้น หากคุณคลิก “ตกลงและค้นพบ KUKA” จะถือว่าคุณยอมรับให้ใช้ข้อมูลคุกกี้เพื่อประโยชน์ทางการตลาด คุณสามารถเลือกได้ว่าจะให้เราใช้ข้อมูลคุกกี้ประเภทใดด้วยการคลิก “การตั้งค่าคุกกี้”

การตั้งค่าคุ้กกี้