Human-robot collaboration enables flexible production processes

The KUKA lightweight robot combines injection molding with additive manufacturing.

25 Tháng Giêng 2016

KUKA system partner automates additive manufacturing system using LBR iiwa

 

The German machinery manufacturer ARBURG has developed a fully automated production line, completely networked in terms of IT processes, which allows series-manufactured injection moldings to be individualized right at the production line, according to the customer’s requirements. To do this, the “freeformer”, ARBURG’s additive manufacturing system, applies customized, plastic lettering and symbols to the molding, resulting in the creation of a unique product. Automation of the freeformer was made possible by KUKA’s system partner, FPT.

Customized office scissor production was demonstrated at the 2015 Fakuma plastics trade fair as a highlight of the key topic “Industry 4.0”. This included: the KUKA LBR iiwa (intelligent industrial work assistant), the world’s first series-produced, sensitive lightweight robot suitable for use in industrial applications, which can interact with humans without requiring a safeguarded zone. This robot combines injection molding with additive manufacturing. The ARBURG host computer system (ALS) plays a central role in the IT networking of the stations.

 

Use of the LBR iiwa enables maximum flexibility at Arburg.

LBR iiwa handles office scissors at injection molding machine


 

When submitting an order for customized office scissors, customers can create their personalized lettering for the handles, etc. on a tablet PC. The signature is thus created digitally and saved on a chip card. This is input into the control system on the injection molding machine and series production begins. As part of this process, the plastic handles are molded onto the stainless steel blades which are loaded by a linear robot system. A unique DM code is lasered onto each product. At this point, the product itself becomes a data and information carrier and is assigned its own website containing all production and quality parameters. A KUKA LBR iiwa then removes one pair of office scissors at a time from the injection molding cell’s conveyor belt together with the workpiece carrier.
The product is identified by a scanner on the basis of its DM code which initiates the next production step. Scissors which are to be individualized with customer-specific lettering are passed to the freeformer by the LBR iiwa. The LBR iiwa communicates with the robot system via a Euromap 67 interface and applies the lettering as a plastic 3D geometrical design onto the scissor handles. The LBR iiwa then removes the customized scissors from the freeformer and passes them to the final quality inspection.

Joint torque sensors ensure safe human-robot collaboration

The KUKA LBR iiwa plays a central role in customizable series production. As the lightweight robot is equipped with seven axes, it is extremely agile and can combine injection molding with additive manufacturing in an optimum fashion. The LBR iiwa is predestined for extremely flexible production concepts due to its low weight and ideal balance of reach and payload capacity. With its highly responsive sensor technology, the LBR iiwa is designed for direct collaboration with its human “colleagues”, yet can also handle sensitive products safely and does not require a safeguarded zone.

This means that skilled workers can pass workpieces to the robot directly, if necessary, which makes the production process even more flexible and saves on space.

Các thiết lập cookie Hãy khám phá OK và KUKA

Trang web này sử dụng Cookie (xem thêm thông tin chi tiết) để cung cấp cho bạn dịch vụ trực tuyến tốt nhất. Nếu bạn tiếp tục sử dụng trang web của chúng tôi, thì chúng tôi chỉ sử dụng Cookie cần thiết về mặt kỹ thuật. Nếu bạn nhấp vào „Hãy khám phá OK và KUKA“, bạn đã đồng ý sử dụng Cookie Marketing. Bằng cách nhấp vào „Các cài đặt Cookie“ bạn có thể chọn Cookie mà chúng tôi sử dụng.

Các thiết lập cookie