激光沉积焊接:工艺技术
激光沉积焊接将高效激光用作热源。通过同时熔化并涂覆几乎任意一种材料产生表面覆层。辅材既可以选用粉状材料(如金属粉末),也可以选用焊丝。在采用粉末进行激光沉积焊接的过程中,激光通常以散焦的方式加热工件,并将其原地熔化。同时输送混合细金属粉末的惰性气体。在加热位置上,金属粉末熔化并与工件表面融合为一体。
Laser metal deposition with the aid of powder-based or wire-shaped filler materials can be used for repair work, the application of wear and corrosion protection, and the production of 3D components (additive manufacturing).
激光沉积焊接将高效激光用作热源。通过同时熔化并涂覆几乎任意一种材料产生表面覆层。辅材既可以选用粉状材料(如金属粉末),也可以选用焊丝。在采用粉末进行激光沉积焊接的过程中,激光通常以散焦的方式加热工件,并将其原地熔化。同时输送混合细金属粉末的惰性气体。在加热位置上,金属粉末熔化并与工件表面融合为一体。
KUKA 能够为您提供个性化的解决方案,以及各种激光沉积焊接生产工艺。从模块化的机器人单元到全自动设备,同时还包括与其他接合工艺相结合。
Discover the hybrid additive manufacturing solution from KUKA. The goal of the ProLMD project is the industrial implementation of hybrid manufacturing processes using laser technology. A Quantec KR 90 HA robot builds up new structures layer by layer on a conventionally manufactured base component. Thanks to the use of a fiber-guided system, the robot remains virtually unrestricted in its workspace. This makes it possible to respond flexibly to component geometry and size – even in the case of small batch sizes. The development of a locally integrated shielding gas system, which is only deployed when required, offers further advantages. This system is supplemented with new laser processing heads, which make use of both wire and powder as filler materials, as well as with a computer-aided manufacturing (CAM) system suitable for hybrid production. Several filler materials are being researched within the framework of ProLMD with a view to developing highly efficient laser material deposition processes.