請選擇您的所在位置:

國家

Major order from the automotive industry

KUKA Systems landed another major automotive industry order in the fourth quarter of 2011

2011年11月30日


A European manufacturer in the premium segment awarded the company its order for the construction of two complete assembly lines. Both sub-orders comprise the engineering, design, construction and commissioning of each system. In addition, individual components such as rear and middle vehicle underbodies will also be manufactured within the scope of this order. The project will integrate industrial robots to manufacture the various components using the spot welding method.

This premium manufacturer's major order has a volume in the medium double-digit million euro range and will be booked pro rata at the end of 2011 and the beginning of 2012.

“Our customer makes the highest demands on the performance capability and flexibility of its production facilities,” emphasizes Dr. Till Reuter, CEO of KUKA AG. “KUKA Systems delivers all of this cutting edge technology from a single source.”

我們使用 Cookie

本網站使用 Cookie (更多相關資訊),以便線上為您提供最佳服務。若您繼續使用我們的網站,我們只使用技術上必要的 Cookie。點選「確定並瞭解 KUKA」,則表示您額外同意使用行銷 Cookie。點選「Cookie 設定」,您可以選擇我們使用哪些 Cookie。

Cookie 設定