請選擇您的所在位置:

國家

KUKA recieves major order from Spanish automotive parts supplier

KUKA Systems GmbH Augsburg won a major order from a Spanish car parts supplier in the second quarter of 2012, to build several highly flexible manufacturing lines

2012年8月3日


The project comprises the entire engineering and construction for four lines that will manufacture car body parts such as front and rear sliding doors and tailgates for various types of vehicles. The contract includes building the pre-production assemblies. The order is valued in the lower double-digit million euro range.

Dr. Till Reuter, CEO of KUKA AG, says: "What's noteworthy about this product is the wide variety of models being assembled and the remote laser welding technology. The latter process enables parts to be welded from a considerable distance using a laser with a very high power density."

我們使用 Cookie

本網站使用 Cookie (更多相關資訊),以便線上為您提供最佳服務。若您繼續使用我們的網站,我們只使用技術上必要的 Cookie。點選「確定並瞭解 KUKA」,則表示您額外同意使用行銷 Cookie。點選「Cookie 設定」,您可以選擇我們使用哪些 Cookie。

Cookie 設定