請選擇您的所在位置:

國家

Volkswagen increasingly commits to KUKA technology

Volkswagen AG is increasingly committing to cutting edge technology from Augsburg. The company awarded a new frame contract for industrial robots to KUKA in the third quarter of 2012.

2012年11月7日


Important large order for KUKA Roboter

Under the terms of the contract, KUKA Roboter GmbH will supply in total 6,000 of its new KR QUANTEC generation of industrial robots, including KR C4 controllers, to various Volkswagen factories in Germany and Eastern Europe in 2013 and 2014. Of the total, 1,800 robots are destined for Emden and Zwickau, where they will be used on production lines for the VW Passat's successor. Audi AG will receive 2,600 units for the new Audi A4, which will be built at Ingolstadt und Neckarsulm. The remaining 1,600 units will be shipped to the Volkswagen plant in Bratislava, Slovakia. The orders from this blanket contract will be booked from now until 2014 as they are released by the customer. 

"We are proud that Europe's largest carmaker is increasingly committing to cutting-edge technology from Augsburg," said Dr. Till Reuter, CEO of KUKA AG, as he commented on the order placement. "After all, 6,000 robots is the highest number of units KUKA has ever received at one time in a blanket order."
 

我們使用 Cookie

本網站使用 Cookie (更多相關資訊),以便線上為您提供最佳服務。若您繼續使用我們的網站,我們只使用技術上必要的 Cookie。點選「確定並瞭解 KUKA」,則表示您額外同意使用行銷 Cookie。點選「Cookie 設定」,您可以選擇我們使用哪些 Cookie。

Cookie 設定