請選擇您的所在位置:

國家

KUKA robot receives prestigious industrial design award

KUKA Robotics has won one of the most prestigious honors in Industrial Design: the Good Design Award.

2014年1月7日


The KUKA robot KR 270 QUANTEC ultra was awarded end of last year in the category "Robotics / Bionics". Initiator of the award is the U.S. Chicago Athenaeum Museum of Architecture and Design in cooperation with the European Centre for Architecture, Art, Design and Urban Studies. Every year, a distinguished jury of design experts selects the winners out of thousands of submissions. One of the most important requirements is that the excellent product is able to enrich society and people's lives.

The Good Design Award is presented annually since 1950 and was originally founded by four American architects. In addition to "Robotics / Bionics" there are several other categories such as textile, furniture, packaging and electronics

www.chi-athenaeum.org/gdesign/

本網站使用 Cookie (更多相關資訊),以便線上為您提供最佳服務。若您繼續使用我們的網站,我們只使用技術上必要的 Cookie。點選「確定並瞭解 KUKA」,則表示您額外同意使用行銷 Cookie。點選「Cookie 設定」,您可以選擇我們使用哪些 Cookie。

Cookie 設定