請選擇您的所在位置:

國家

KUKA wins major automotive contract

Daimler AG is increasingly investing in leading-edge technology products from Augsburg. For the body-in-white production of the new C-class, Daimler has awarded a major contract to KUKA. The order value was booked in the third quarter of 2018.

2018年10月29日


Production systems for the front and rear end, as well as the underbody line, will be built for a number of derivatives. A total of around 800 industrial robots from the KR QUANTEC series, complete with the KR C4 controller, will be integrated at the plants, together with various AGVs that round out the flexible production concept.

“We are delighted that our longstanding customer with its demanding technical standards has once again opted for KUKA,” emphasizes Dr. Till Reuter, CEO of KUKA AG. “This contract is recognition of our innovative technologies and products.”

消息下載

下載 PDF

本網站使用 Cookie (更多相關資訊),以便線上為您提供最佳服務。若您繼續使用我們的網站,我們只使用技術上必要的 Cookie。點選「確定並瞭解 KUKA」,則表示您額外同意使用行銷 Cookie。點選「Cookie 設定」,您可以選擇我們使用哪些 Cookie。

Cookie 設定