請選擇您的所在位置:

國家

Strategic alliances: "Achieving individual goals better together"

Driving digital transformation with strong partners

2021年5月10日


It's about the end-to-end connectivity within the industry: from the machine, via the edge to the cloud, and right into the ERP-system. It is difficult to be a specialist in each of these disciplines, and often not cost-effective either. Close partnerships are needed to ensure that end-to-end industrial digitalization from the machine to the cloud works. KUKA is working with SAP, Microsoft, Siemens and around 80 other member companies in the Open Industry 4.0 Alliance to drive the connectivity within the industry forward.

Digitization in industry will only work if companies also leave their own path to some extent in order to create something great together in ecosystems

Dr. Christian Liedtke, Head of Strategic Alliances
Industry 4.0 celebrates its 10th anniversary this year. Over the past ten years, it has become clear above all that connectivity and digitization within industry require a level of perfection in theory that is rarely found in practice behind the factory gates. Industry 4.0 means connectivity. But Industry 4.0 also means complexity. The big challenge is how to connect different machines. Interfaces exist, but they are not yet seamless. "Industry 4.0 applications are not scalable today. The communication of the individual components must be coordinated individually with each machine supplier. In the Open Industry 4.0 Alliance, we rely on open standards and interfaces to actually transfer Industry 4.0 into practice," says Dr. Liedtke.

„Fish swim in swarms to appear bigger and more dangerous for their enemies“

Why it makes sense to harness the power of community. “3 questions, 3 answers” and with Dr. Christian Liedtke.

我們使用 Cookie

本網站使用 Cookie (更多相關資訊),以便線上為您提供最佳服務。若您繼續使用我們的網站,我們只使用技術上必要的 Cookie。點選「確定並瞭解 KUKA」,則表示您額外同意使用行銷 Cookie。點選「Cookie 設定」,您可以選擇我們使用哪些 Cookie。

Cookie 設定