Major order from Ford

KUKA receives major order from Ford in Spain to automate a body-in-white line

2011年10月20日

KUKA Systems has received a major order from Ford in Europe. Under the terms of the contract, the division will automate a body-in-white line for the successor to the Ford KUGA at the company’s plant in Valencia, Spain.

As part of this order, KUKA Systems will deliver manufacturing systems for components such as doors, fenders, engine hoods and tailgates. The parts will be welded, glued or folded at upstream manufacturing cells and then automatically sent to the body-in-white assembly line for the new Ford KUGA, thereby improving the line’s efficiency. After the upgrade has been completed in the first half of 2012, the line will be capable of producing a considerably higher number of vehicles. The value of the order, which was booked in the third and fourth quarters of 2011, is in the lower double-digit million euro range.

Especially impressive is the fact that the systems and tools are being installed without shutting down the existing line. "This technically challenging project order from a long-standing and important automotive customer demonstrates that KUKA Systems earns high marks for quality,” said KUKA AG’s CEO Dr. Till Reuter.

Cookie 設定 確定並瞭解 KUKA

本網站使用 Cookie (更多相關資訊),以便線上為您提供最佳服務。若您繼續使用我們的網站,我們只使用技術上必要的 Cookie。點選「確定並瞭解 KUKA」,則表示您額外同意使用行銷 Cookie。點選「Cookie 設定」,您可以選擇我們使用哪些 Cookie。

Cookie 設定