KUKA at K 2019

The plastics industry is booming. Nevertheless, it is still facing challenges: at K 2019, KUKA is presenting various solutions for responding to these challenges. The world’s leading trade fair for the plastics and rubber industry is being held in Dusseldorf from 16 to 23 October.

2019年9月27日

Visit us at K 2019: Hall 12, Booth B35

KUKA is exhibiting at this year’s K trade fair under the motto “industrial intelligence in automation _ products and expertise for the plastics industry”. One highlight at the KUKA trade fair booth is an environmentally-friendly set of reusable cutlery that is being handed out to trade fair visitors. The key machining operations on the cutlery are performed by the flexobot robotic cell. The cell is centered on a KUKA KR 10 R900-2 robot. It is ideally suited to cooperation with injection molding machines.

Clean and flexible material handling with a CO₂ laser robot 

CO₂ laser cutting enables the automated 3D cutting and perforation of workpieces made from a range of different plastics. Another topic being showcased is the robotic solution for the extrusion of thermoplastic elastomer 

Experience KUKA at K 2019

Find out further details about our trade fair applications and speak with our KUKA experts for the plastics industry on site.

Get your free admission ticket
Cookie 設定 確定並瞭解 KUKA

本網站使用 Cookie (更多相關資訊),以便線上為您提供最佳服務。若您繼續使用我們的網站,我們只使用技術上必要的 Cookie。點選「確定並瞭解 KUKA」,則表示您額外同意使用行銷 Cookie。點選「Cookie 設定」,您可以選擇我們使用哪些 Cookie。

Cookie 設定