請選擇您的所在位置:

國家

Solderen

Laser soldering

Laser soldering enables substance-to-substance bonds. The laser can be focused with high accuracy. This means that even the smallest solder joints and sensitive electronic components can be connected. The technology is also frequently used in the automotive industry or in the electronics sector.


Laser soldering: the technology

Laser soldering is a non-contact process: the laser beam heats up the solder. This is then introduced to the process as a filler wire, which usually consists of copper or zinc alloys. The solder then melts and fills the joint gap. The melt fuses the two components.

Laser soldering is subdivided into two variants:

  1. Laser hard soldering, or laser brazing, with melting temperatures above 450 degrees Celsius:
    This joining technique uses diode lasers with higher power and is used primarily in the automotive industry.
  2. Soft laser soldering with melting temperatures below 450 degrees Celsius:
    This technique is commonly used in the manufacture of electronic components.

Automated laser soldering

As a KUKA customer, you have two options:

  • Automated and scalable production systems
  • Individually configured manufacturing cells

Parameters such as path velocity, laser power or optimum wire feed are second nature to us, and we offer various technology packages for different production scenarios.

Laser soldering in the process

Laser soldering in the process

本網站使用 Cookie (更多相關資訊),以便線上為您提供最佳服務。若您繼續使用我們的網站,我們只使用技術上必要的 Cookie。點選「確定並瞭解 KUKA」,則表示您額外同意使用行銷 Cookie。點選「Cookie 設定」,您可以選擇我們使用哪些 Cookie。

Cookie 設定