Showcase at LogiMAT 2026: KUKA presents mobile robotics in an interactive arena
Visitors to LogiMAT 2026 in Stuttgart (24 to 26 March) will experience a special showcase covering more than 600 square meters: In the ‘Interoperability Arena’, KUKA and partners such as SYNAOS, WIFERION and FPT Robotik will demonstrate the interaction between autonomous vehicles and 6-axis industrial robotics.
10 กุมภาพันธ์ 2569
Interaction between AMR and stationary robots
Experience the collaboration between AMR and robotics systems live
We are very pleased to be at LogiMAT 2026 together with strong partners such as SYNAOS and WIFERION to show how mixed fleets of AMRs are orchestrated on the basis of cloud-based control software and work together efficiently with stationary robot systems in practice.
Visit us at LogiMAT 2026
Visitors will have the opportunity to talk to KUKA representatives and partners about possible applications. The intelligent software solution KUKA.AMR Fleet will also be presented live on site.
Two other members of the KUKA Group will also be represented at LogiMat 2026: Intralogistics professional Swisslog will be demonstrating the advantages of seamlessly integrated automation and software in hall 1, booth B41, under the motto ‘Ready for the Next’. And since digital planning and simulation play an important role in this, Visual Components, the KUKA Group's manufacturing simulation software company, will also be in Stuttgart. In hall 8, booth D80, visitors can see how logistics systems and production processes can be planned, validated and optimized using 3D simulation before implementation.
Flexible, scalable, robust
The Interoperability Arena demonstrates how open standards and intelligent orchestration make material flows more flexible, scalable and robust – a key issue for the intralogistics of tomorrow. For KUKA, as an innovation leader in mobile robotics, LogiMAT is an ideal platform to demonstrate to users and partners how we can jointly drive forward the digitalization and automation of logistics.