เลือกตำแหน่งที่ตั้งของคุณ:

สถานที่

กรุณาเลือกภาษา:

KUKA Group showcases the bridge from industrial automation to Physical AI at NVIDIA GTC Berlin

At NVIDIA GTC Berlin, KUKA and Visual Components are showcasing technologies that connect virtual planning, intelligent perception and physical automation, laying key foundations for the next generation of AI-powered manufacturing.

21 ตุลาคม 2569


Augsburg/ Berlin, Germany, October 21, 2026 – KUKA Group is demonstrating how simulation, AI, software and industrial automation are converging to help manufacturers bridge the gap between digital intelligence and real-world industrial execution. 

Physical AI will fundamentally change how industrial systems are designed, programmed and operated. The challenge now is not only creating intelligent models, but enabling them to operate safely, reliably and productively in real manufacturing environments. This requires a bridge between today's proven industrial automation and tomorrow's AI-driven systems. At KUKA Group we are calling this transformation Automation 2.0 and we are building that bridge through software platforms, simulation, robotics and AI.

Christoph Schell, CEO KUKA Group
KUKA Group Technology Takes Center Stage: KUKA robots were featured in NVIDIA CEO Jensen Huang’s keynote address at NVIDIA GTC 2026 in Berlin, alongside a simulation project by Visual Components and Swisslog.

From Simulation to Execution: Building the Bridge to Physical AI

At GTC Berlin, Visual Components, a specialist in 3D manufacturing simulation and robot offline programming, is presenting FactoryLens, a new viewport built directly into its simulation platform, powered by NVIDIA Omniverse libraries.

Developed as the latest step in Visual Components' collaboration with NVIDIA, FactoryLens lets manufacturers take the factory layouts they already use for simulation and move directly into a more realistic digital-twin environment, with real-time rendering in the software they already use. Today's advanced manufacturing equipment, processes, and facilities are increasingly designed and tested first in simulation, and that validation is only as useful as how closely it reflects the real world. Visual Components provides 3D simulation software that lets manufacturers plan, validate, and optimise factory layouts before they are built, and FactoryLens extends those existing workflows into a more realistic digital-twin environment, inside the platform they already know. Rather than recreating factory models in separate visualization software, users can visualise their large-scale layouts in real time, control materials and appearance, record high-quality video, and export factory configurations using Universal Scene Description (OpenUSD) for use in compatible external environments, all without leaving Visual Components. 

FactoryLens extends existing simulation workflows into a more realistic digital twin environment with real-time rendering. © KUKA Group

KUKA Advances Physical AI with Intelligent Vision Technology

KUKA is also showcasing iiQKA.AI Vision, an AI-enabled vision solution powered by the NVIDIA Jetson Orin module and integrated directly into the KUKA controller environment. The solution enables robots and automation systems to identify objects, detect variations and interpret complex visual information more intelligently. This helps manufacturers to increase flexibility, improve quality and automate tasks that traditionally require significant human intervention or additional hardware. AI-powered perception is a key prerequisite for Physical AI because it enables automation systems to better understand and respond to real-world conditions.

iiQKA.AI Vision enables robots and automation systems to identify objects, detect variations and interpret visual information more intelligently. © KUKA Group

KUKA AMP Orchestrates the Future of Intelligent Automation

While simulation creates the virtual foundation for Physical AI, KUKA Group is also developing software platforms that connect digital intelligence with industrial execution. KUKA unveiled KUKA AMP (Automation Management Platform) at NVIDIA GTC 2026 in March in San Jose and in July KUKA has successfully launched KUKA AMP at KUKA Toledo Production Operations (KTPO) in Ohio, marking a key milestone in bringing AI-powered automation into live automotive production. KUKA AMP enables the integration, management and orchestration of automation assets across different environments. Together with advanced simulation capabilities such as FactoryLens and AI-enabled applications such as iiQKA.AI Vision, platforms like KUKA AMP help manufacturers move from isolated automation systems toward increasingly connected, intelligent and adaptive automation environments.

Our customers are not looking for AI experiments. They are looking for practical pathways to deploy AI safely and productively. Our role is to help them bridge the gap between today's highly reliable automation systems and tomorrow's intent-based manufacturing environments. That transition will not happen overnight, but it is already underway.

Christoph Schell, CEO KUKA Group

Automation 2.0: KUKA's vision for Physical AI

As an end-to-end automation solution provider, KUKA Group defines Automation 2.0 as the pathway to Physical AI: the evolution from traditional deterministic automation toward intelligent, intent-driven systems enhanced by AI. Rather than replacing proven industrial automation principles, Automation 2.0 extends them with perception, contextual understanding and adaptive decision-making capabilities, enabling machines and robots to better understand their environment, learn from operational data and act autonomously. With a portfolio spanning robotics, warehouse and healthcare automation, simulation, software, intralogistics and systems integration, KUKA Group is uniquely positioned to connect every stage of the automation lifecycle, from virtual design and validation to intelligent physical execution, creating the foundation for Physical AI at industrial scale.

About Visual Components

As part of KUKA Group since 2017, Visual Components brings more than 25 years of expertise in 3D manufacturing simulation and offline robot programming, helping manufacturers connect virtual planning with real-world production.

Download Press Kit

Download the press release and media assets here.