自分の現在地を選択してください:

場所

Sustainability Insights: More sustainable production thanks to simulation

Want to produce more efficiently and conserve resources? This is only possible with the help of state-of-the-art technologies – such as simulation.


Teresa Scheunert
2025年8月14日
Society
読了時間: 3分間

How will a new robot fit into my production process? And how can I optimize its workflow, also with regard to energy consumption? Simulation tools help answer precisely these questions – and combine sustainability with more economical production. Christian Schletter, Product Manager für Engineering and AI Services at KUKA, gives us an overview in the new issue of our Sustainability Insights:

But what does this look like in concrete terms for customers? An exciting example is HASE Kaminofenbau. At this stove manufacturer in southern Germany, welding robots and digital twins work together. The simulation software brings robot applications to life virtually – even before the system is put into operation. The offline-programmed robot motion sequences are mapped and optimized in real time: Read the full story here.

次の記事

こちらもチェックしてみてください