Two tools for even better user guidance in the my.KUKA Marketplace
Even more individual, faster and simpler: two new tools in the my.KUKA Marketplace now guide KUKA customers through the planning and purchasing process in an even more detailed and clearer way. While the AI co-pilot kAIsa recommends customized software products that meet users' needs, the Simulation Assistant allows users to simulate the use of robots and their interaction with accessories.
14 Tháng Ba 2025
This is how the Simulation Assistant works
Robotics can now be experienced by KUKA customers even before they buy. Registered users in the my.KUKA Marketplace can use the new Simulation Assistant tool to visualize the operation of various combinations of applications, robot families and tools. Users are intuitively guided through a four-stage selection process, while the visualization is updated at each step. At the end, it can be saved. The simulation can then be accessed by the customer at any time via the personal project list on my.KUKA.
kAIsa: first AI co-pilot available for customers
The AI assistant kAIsa also provides even more individual user guidance in the my.KUKA Marketplace. Its intuitive application does not require any special technical knowledge on the part of the user. This is because it uses AI technologies to understand the needs and requirements of users. KUKA customers can simply describe their specific use case in natural language in an exchange with kAIsa. The AI co-pilot then analyzes the information and ultimately recommends the most suitable simulation products. Users also have the option of purchasing the recommended product directly in the my.KUKA Marketplace.
kAIsa also guarantees the compatibility of the robotic product and operating system at all times. In terms of security, the AI co-pilot also meets the highest standards: kAIsa has no access to KUKA company data; the AI co-pilot works exclusively with information that has been provided in a protected database. This makes it even easier and faster for KUKA customers to receive personalized, tailored product recommendations in a protected environment. In order to be able to discuss these with a representative from KUKA Sales, suggested appointments are offered during the process.